Post Go back to editing

Migrating project from VisualDsp++ to CrossCore ADSP-21363

Hello,

I need to port a VisualDSP Project to CrossCore Embedded Studio. I used the CrossCore import VisualDSP Project

method. Firstly, when I tried build the project it throws out the Linker Error: 

When I copied libraries from VisualDsp++ and added library path with this files, now I have Erorr:

<?xml version="1.0" standalone="no"?>
<?xml-stylesheet type="text/xsl" href="file:///E:/Analog Devices/CrossCore Embedded Studio 2.4.0/System/linker_log.xsl"?>
<DOCUMENT gen_time='Mon Nov 21 01:50:44 2016
'>
<MSG id='00964E30' mid='li1032' type='Error' >
<TEXT><![CDATA['363_hdr.doj' is not a valid input file.]]></TEXT>
</MSG>
</DOCUMENT>

Maybe you can point something out to help me track the problem down. If you need further Information, please let me now. In attachment I added mine project, added libraries and ldf file, which I'm using.

 

Sincerley,

Tomasz

Parents
  • Hi Tomasz,

    We understand that you are facing li1032 linker error. This error will occur when an input file to the link cannot be read by the linker. The linker processes ELF object files. The file named is not a valid ELF object file.Please confirm that the file being read is a valid ELF file produced by CCES tools.

    For reference please refer the below CCES help path:
    CrossCore Embedded Studio <version> > Blackfin Development Tools Documentation > Linker and Utilities Manual > Linker and Archiver Messages > Linker Messages > Errors > li1030

    Also please refer the following Ezone links:

    https://ez.analog.com/docs/DOC-2466

    https://ez.analog.com/message/76623

    Best Regards,

    Kader

Reply
  • Hi Tomasz,

    We understand that you are facing li1032 linker error. This error will occur when an input file to the link cannot be read by the linker. The linker processes ELF object files. The file named is not a valid ELF object file.Please confirm that the file being read is a valid ELF file produced by CCES tools.

    For reference please refer the below CCES help path:
    CrossCore Embedded Studio <version> > Blackfin Development Tools Documentation > Linker and Utilities Manual > Linker and Archiver Messages > Linker Messages > Errors > li1030

    Also please refer the following Ezone links:

    https://ez.analog.com/docs/DOC-2466

    https://ez.analog.com/message/76623

    Best Regards,

    Kader

Children
No Data