ADSP-21364 EZ-KIT Lite and CrossCore debugging/connection problems

Hello,

I have an ADSP-21364 EZ-KIT board and I am struggling to connect to it using CrossCore. I am using Crosscore 2.7.0 on a Windows 7 x86 version (because I could not find any drivers for the board for x64 system, I used the VisualDSP++ drivers and they worked on x86). I tried to load, via USB, and debug a sample project. I had downloaded the Board Support Package for ADSP-21364 and configured the debugger to target this specific board. The device is listed on Windows Device Manager as ADI Development Tool and the USB_MONITOR Led on board is lighted up.

Still, when I tried to debug the program with debug configuration set-up as ADSP-21364 EZ-KIT board, I got such error:

[TpsdkServer] Failed to connect to processor.

Error: 0x80048020
Error Description: Selected emulator not detected


Using the Target Configurator -> Test tool, it failed on Opening Emulator Interface.

Do someone have an idea what could go wrong? Are there somewhere drivers for x64 architecture for this specific board?

Thanks in advance for any help

  • 0
    •  Analog Employees 
    on Feb 27, 2018 4:27 PM

    Hi,

    Can you please confirm that your using Emulator or SADA2 to debug the target. If are using SADA2 CCES includes a new device driver which adds support for the ICE-1000 and ICE-2000 products. This driver differs from previous releases, and requires that the jumpers on the ICE-100B or SADA-II board are adjusted as detailed in the following FAQ:
    https://ez.analog.com/docs/DOC-11226

    Can you please check that the SADA is installed properly by checking their computer 'Device Manager'. You should find the EZ-Board listed under 'CrossCore Tools'. If listed, double-click on it to show the driver properties and ensure there are no issues listed.If the EZ-Board is not listed or having problems with the drivers, Please try reinstalling the drivers.

    Please refer "Installing Drivers Manually" to manually uninstall your driver and manually install new ones:
    http://www.analog.com/media/en/technical-documentation/application-notes/EE356.pdf

    If still you are facing any issue can you please share the below details:
    1.Please share the screenshot of device manger.
    2.Share us the image which shows your board connected with SADA 3.ICE test results and error message if any.
    4.Please confirm that you were able to debug the simple program successfully.
    5.Are you received "Failed to connect to processor" error for every time of Debug the target?

    Regards,

    Kader

  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:02 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin