When I add "μC/OS-III RTOS for SHARC" to my working project (spdif audio playback) I get ADI_ADAU1962A_TWI_ERROR when initializing the DAC.
I have only added the Micrium stuff to the project, not done any calls at all.
Any suggestions?
I added the uCOS in system.svc to a newly created "spdif playback" project from the examples, and started the debugger. This is the output:
Loading application: "C:\Analog Devices\CrossCore Embedded Studio 2.7.0\SHARC\ldr\ezkitSC573_preload_core0"Load complete.Loading application: "C:\Users\more10\git\micrium-test\examples\sc58x_ez_kit_2.0.2\SPDIF Audio Playback (SC573 SHARC)\SC573\sharc\spdif_playback_Core0\Debug\SPDIF_Playback_SC573_SHARC_Core0"Load complete.Loading application: "C:\Users\more10\git\micrium-test\examples\sc58x_ez_kit_2.0.2\SPDIF Audio Playback (SC573 SHARC)\SC573\sharc\spdif_playback_Core1\Debug\SPDIF_Playback_SC573_SHARC_Core1.dxe"Load complete.Loading application: "C:\Users\more10\git\micrium-test\examples\sc58x_ez_kit_2.0.2\SPDIF Audio Playback (SC573 SHARC)\SC573\sharc\spdif_playback_Core2\Debug\SPDIF_Playback_SC573_SHARC_Core2.dxe"Load complete.adi_twi_Write failedadi_twi_Write failedadi_twi_Write failedadi_twi_Write failedadi_twi_Write failedadi_twi_Write failedadi_twi_Write failedadi_twi_Write failedADAU1962A: Failed to configure DAC power, Error Code: 0x00000008Error