Post Go back to editing

CrossCore Serial Flash Programmer UART boot option "Load & Run" not working on ADSP-SC835 SOM

Category: Software
Product Number: CrossCore Serial Flash Programmer
Software Version: 1.8.0

Hello,

I have the ADSP-SC835 SOM and wanted to test starting my application on the DSP via UART boot. For this, I got the CrossCore Serial Flash Programmer and tried to upload the loader file to the board with the option "Load & Run". This always failed, after some time the SYS_FAULT LED was on, but my program on the DSP was not running. First I believed something is wrong in my firmware project until I tried to load the loader file of the blinky example (ADSP-SC83x-Blinky.ldr) shipped with the Flash Programmer and run into the same issue.

The interesting thing is, the download of the loader file to the processor is always working fine, but firmware doesn't start running:

If I keep everything the same and just switch to "Program" instead of "Load & Run", everything works fine. Firmware is downloaded and after setting boot mode to SPI and processor reset the LEDs are blinking as expected.

Can you please tell me what I did wrong when trying to directly boot the firmware via UART without writing it to flash via second stage kernel? Is it a bug in Cross Core Serial Flash Programmer?

Thanks for your help in advance!

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.