Post Go back to editing

CrossCore Serial Flash Programmer UART boot option "Load & Run" not working on ADSP-SC835 SOM

Category: Software
Product Number: CrossCore Serial Flash Programmer
Software Version: 1.8.0

Hello,

I have the ADSP-SC835 SOM and wanted to test starting my application on the DSP via UART boot. For this, I got the CrossCore Serial Flash Programmer and tried to upload the loader file to the board with the option "Load & Run". This always failed, after some time the SYS_FAULT LED was on, but my program on the DSP was not running. First I believed something is wrong in my firmware project until I tried to load the loader file of the blinky example (ADSP-SC83x-Blinky.ldr) shipped with the Flash Programmer and run into the same issue.

The interesting thing is, the download of the loader file to the processor is always working fine, but firmware doesn't start running:

If I keep everything the same and just switch to "Program" instead of "Load & Run", everything works fine. Firmware is downloaded and after setting boot mode to SPI and processor reset the LEDs are blinking as expected.

Can you please tell me what I did wrong when trying to directly boot the firmware via UART without writing it to flash via second stage kernel? Is it a bug in Cross Core Serial Flash Programmer?

Thanks for your help in advance!

  • Hi,

    Thank you for your inquiry.

    We are looking into your query now. We will get back to you.

    Best Regards,
    Santhakumari.V

  • Hi Leonhard,

    In order to isolate the issue, could you please share the below details:

    1. Which revision of the ADSP-SC835-SOM board are you currently using?

    2. If Rev A, have you followed the instructions from CrossCore Serial Flash Programmer Users Guide Chapter 3.11, “ADSP21835W-EV-SOM and ADSPSC835W-EV-SOM Board Modification,” from CrossCore Serial Flash Programmer (CCSFP) installation directory? The PDF is available at the following path:
    [Installation Directory]:\Analog Devices\CrossCoreUtilities-Rel1.8.0\Docs\CrossCoreSerialFlashProgrammer_UsersGuide.pdf

    3. Is this your first time you are facing the issue in ADSP-SC835-SOM board, or were you able to successfully use the “Load & Run” option previously?

    Waiting for your reply.

    Best Regards,
    Santhakumari.V

  • Hi Santhakumari,

    I have Rev A of the SOM and followed the relevant steps of the user guide:

    • R28 shorted
    • placed 10k resistor on R82 and R84 (I know, the manual says 20k but both values will result in a logic low signal in the voltage divider with the 100k pullups (R81, R83)

    Since the option "Program" where the flash is programmed via UART and second stage bootloader is working, I think the board modifications are not the problem.

  • Hi,

    We are checking this query with our Internal team. We will get back to you once we get a response from them.

    Best Regards,
    Santhakumari.V

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.