Issue Description Example and Setup Description:
The Winbond W25Q256JV serial flash (expected JEDEC ID EF 4019) programs correctly from the on-board S32K322 MCU, proving the flash device is healthy.
However, I am unable to read the JEDEC/Manufacturer ID from the ADSP-21835W (DSP0) over SPI2. MOSI transmits the 9F 00 00 00 read-ID command correctly, the chip-select (PA05) toggles, and SCLK is present, but MISO stays high (reads back 0xFF) — the flash never drives the bus. When execute the target side algo example get the error
"Error detected in algorithm command execution. Closing down algorithm"

Board / Setup:
- Board: EA3 dual soc board with two processors sharing one SPI serial-flash bus:
- DSP0 = ADSP-21835W (SHARC-FX, primary) — the master I am trying to program from.
DSP1 = ADSP-SC59xW (secondary) — held in reset, so it stays off the shared bus. - Flash: Winbond W25Q256JV, 32 MiB, connected to SPI2 and shared between DSP0 and DSP1.
- Cross-check master: S32Kxx MCU (programs the same flash successfully).
- Toolchain: CCES 3.1.0, cldp.exe + OpenOCD (adsp2183x flash driver), ICE-2000 JTAG emulator.
- Firmware: Target-side g_cfg flash algorithm (2183x_flash), ported/aligned to the working 2156x DPIA reference flasher. SPI2 mode 0, 8-bit words, PA05 as manual GPIO CS (idle high), PA00–PA04 muxed to SPI2 (MISO/MOSI/D2/D3/CLK). ( link for algo ADSP-SC835/21835 SHARC FX and ADSP-SC594 Family Cortex A5 Custom Flash Drivers - FAQs - CrossCore Embedded Studio and Add-ins - EngineerZone)
What I have already verified:
- MOSI/CLK/CS confirmed correct on the analyzer
- Same flash programs fine from the S32Kxx MCU.

Questions:
- Is this correct — that for the ADSP-21835 the supported programming path is CLDP → OpenOCD cfg → target-side g_cfg algorithm, and there is no CLDP + DPIA (AFP) path as on the 21569/SC593? If a DPIA-style flow is available for the 2183x, please point me to the example; otherwise please confirm the OpenOCD + g_cfg algorithm is the intended method.
- What does "Could not read device id" point to? Is it that OpenOCD loaded the algorithm, but the g_cfg handshake never completed — i.e. no valid device ID was written back before OpenOCD's read timeout?