Hi,
We verified the Flash update process on an ADI evaluation board (ADSP21835-EV-SOM + EV-SOMCRR-EZKIT) using the latest version, CCES 3.1.0.
However, we encountered an issue where a timeout occurs during the Flash write operation following the Flash erase. Could you please advise on the possible causes?
Software verified:
A timeout occurs during the Flash write operation after the Flash erase when using the BSP's "Talkthrough" sample project.
Flash writing works without issues in CCES 3.0.4.
Therefore, we suspect this issue may be related to the update to CCES 3.1.0.
For reference, here are the logs from CCES 3.1.0 and CCES 3.0.4.
CCES 3.1.0:
Downloading to device...
'Invoking: CrossCore SHARC-FX Device Programmer'
cldp -proc ADSP-21835 -verbose -cmd prog -driver "C:\analog\cces\3.1.0\ARM\openocd\share\openocd\scripts\board\flash_algorithms\2183x_flash.dxe" -erase all -emu KIT -format hex -board adsp21835w_ev_som.cfg -file "AD_TalkT_I2S_EZ_21835_Core1.ldr"
Processor ADSP-21835
Board Cfg File adsp21835w_ev_som.cfg
Emulator KIT
Using OpenOCD.
Selected the following configuration files to run OpenOCD:
interface/adi-dbgagent.cfg
board/adsp21835w_ev_som.cfg
Creating child process to run OpenOCD.
Command line used internally:
C:\analog\cces\3.1.0\ARM\openocd\bin\openocd.exe -c "tcl_port 6666" -c "telnet_port 4444" -c "gdb_port 3333" -f "interface/adi-dbgagent.cfg" -f "board/adsp21835w_ev_som.cfg" -d0
OpenOCD running as expected.
Connecting to OpenOCD server on TCL.
Successfully connected to OpenOCD server.
Putting socket into non-blocking mode.
Current Algorithm version for selected device is 260625
Program AD_TalkT_I2S_EZ_21835_Core1.ldr
Erasing all device flash. This may take a couple of minutes.
.................................................
Using hex format does not allow for multiple flash devices using same address. Only first flash bank specified at address will be used.
Writing program data to flash.
..............
Timeout during algorithm command execution
Cannot read from flash. Target is not halted!
auto_probe failed
Command done. Check console above for results.
Terminating OpenOCD process
Closing socket.
'Finished building: program_device'
' '
CCES 3.0.4:
Downloading to device...
'Invoking: CrossCore SHARC-FX Device Programmer'
cldp -proc ADSP-21835 -verbose -cmd prog -driver "C:\analog\cces\3.0.4\ARM\openocd\share\openocd\scripts\board\flash_algorithms\2183x_flash.dxe" -erase all -emu KIT -format hex -board adsp21835w_ev_som.cfg -file "AD_TalkT_I2S_EZ_21835_Core1.ldr"
Processor ADSP-21835
Board Cfg File adsp21835w_ev_som.cfg
Emulator KIT
Using OpenOCD.
Selected the following configuration files to run OpenOCD:
interface/adi-dbgagent.cfg
board/adsp21835w_ev_som.cfg
Creating child process to run OpenOCD.
OpenOCD running as expected.
Connecting to OpenOCD server on TCL.
Successfully connected to OpenOCD server.
Putting socket into non-blocking mode.
Use boot mode 0 for most reliable flashing.
Current Algorithm version for selected device is 241209
Program AD_TalkT_I2S_EZ_21835_Core1.ldr
Erasing all device flash. This may take a couple of minutes.
.................................................
Using hex format does not allow for multiple flash devices using same address. Only first flash bank specified at address will be used.
Writing program data to flash.
.
wrote 92180 bytes from file AD_TalkT_I2S_EZ_21835_Core1.ldr in 1.052600s (85.521 KiB/s)
Command done. Check console above for results.
Terminating OpenOCD process
Closing socket.
'Finished building: program_device'
' '
Best regards.