Post Go back to editing

How to access the hardware break/watchpoints (SWU) for SC835

Thread Summary

The user asked if hardware breakpoints/watchpoints can be accessed in CCES for the SC83x. The final answer indicates that the GUI functionality is broken, but a workaround involves manually setting up the SWU registers via the Debugger Console. The accompanying answer confirms that adding a C/C++ Watchpoint in the expressions window does not provide a hardware option and does not trigger a breakpoint on value modification.
AI Generated Content
Category: Software
Software Version: CCES 3.0.3

Is it possible to access the hardware breakpoints / watchpoints in CCES for the SC83x ? 

I see that the SWU regs are populated in the Peripherals window, do I have to set the regs up manually ?

Thanks