I'm using CCES 3.0.3 with an ICE-1000 and an ADSPSC835W-EV-SOM on the EV-SOMCRR-EZKIT.
I'm using a launch group which runs the preload & loads cores 1&2. 50% of the time it works fine, but the other 50% I get..
Error in final launch sequence: Failed to execute MI command: -target-select remote localhost:3333 Error message from debugger back end: localhost:3333: Connection timed out. Failed to execute MI command: -target-select remote localhost:3333 Error message from debugger back end: localhost:3333: Connection timed out. localhost:3333: Connection timed out.
It seems a lot more unreliable than previous systems.
The preload OpenOCD console shows
Open On-Chip Debugger (Analog Devices 0.12.0-1.2.0) OpenOCD 0.12.0 (2025-04-03-09:09) Licensed under GNU GPL v2 Report bugs to <processor.tools.support@analog.com> 0 adapter speed: 5000 kHz Info : auto-selecting first available session transport "jtag". To override use 'transport select <transport>'. Info : xtensa permissive mode is disabled adapter speed: 5000 kHz Info : Listening on port 6666 for tcl connections Info : Listening on port 4444 for telnet connections Info : ICE-1000 firmware version is 1.0.2 Info : clock speed 5000 kHz Info : JTAG tap: adspsc83x.adjc tap/device found: 0x0282c0cb (mfg: 0x065 (Analog Devices), part: 0x282c, ver: 0x0) Info : JTAG tap: adspsc83x.cpu enabled Info : [adspsc83x.apb] Examination succeed Info : [adspsc83x.axi] Examination succeed Info : [adspsc83x.ahb] Examination succeed Info : [adspsc83x.sharcfx] Examination succeed Info : [adspsc83x.m33] Cortex-M33 r1p0 processor detected Info : [adspsc83x.m33] target has 8 breakpoints, 4 watchpoints Info : [adspsc83x.m33] Examination succeed Info : gdb port disabled Info : gdb port disabled Info : gdb port disabled Info : starting gdb server for adspsc83x.sharcfx on 3333 Info : Listening on port 3333 for gdb connections Info : starting gdb server for adspsc83x.m33 on 3334 Info : Listening on port 3334 for gdb connections Info : accepting 'gdb' connection on tcp/3333 Info : [adspsc83x.sharcfx] Debug controller was reset. Info : [adspsc83x.sharcfx] Core was reset. Info : [adspsc83x.m33] external reset detected system reset complete Info : New GDB Connection: 1, Target adspsc83x.sharcfx, state: halted Info : dropped 'gdb' connection Info : accepting 'telnet' connection on tcp/4444 Info : dropped 'telnet' connection
When this starts happening, I have to quit CCES, power cycle the board & ICE several times to get comms back up & running.
The debug window shows

Can you advise how to make this more reliable ?
When it does work, the console shows
Open On-Chip Debugger (Analog Devices 0.12.0-1.2.0) OpenOCD 0.12.0 (2025-04-03-09:09) Licensed under GNU GPL v2 Report bugs to <processor.tools.support@analog.com> 0 adapter speed: 5000 kHz Info : auto-selecting first available session transport "jtag". To override use 'transport select <transport>'. Info : xtensa permissive mode is disabled adapter speed: 5000 kHz 1 Info : Listening on port 6666 for tcl connections Info : Listening on port 4444 for telnet connections Info : ICE-1000 firmware version is 1.0.2 Info : clock speed 5000 kHz Info : JTAG tap: adspsc83x.adjc tap/device found: 0x0282c0cb (mfg: 0x065 (Analog Devices), part: 0x282c, ver: 0x0) Info : JTAG tap: adspsc83x.cpu enabled Info : [adspsc83x.apb] Examination succeed Info : [adspsc83x.axi] Examination succeed Info : [adspsc83x.ahb] Examination succeed Info : [adspsc83x.sharcfx] Examination succeed Info : [adspsc83x.m33] Cortex-M33 r1p0 processor detected Info : [adspsc83x.m33] target has 8 breakpoints, 4 watchpoints Info : [adspsc83x.m33] Examination succeed Info : gdb port disabled Info : gdb port disabled Info : gdb port disabled Info : starting gdb server for adspsc83x.sharcfx on 3333 Info : Listening on port 3333 for gdb connections Info : starting gdb server for adspsc83x.m33 on 3334 Info : Listening on port 3334 for gdb connections Info : accepting 'gdb' connection on tcp/3333 Info : New GDB Connection: 1, Target adspsc83x.sharcfx, state: halted Info : accepting 'telnet' connection on tcp/4444 Info : dropped 'telnet' connection Info : accepting 'gdb' connection on tcp/3334 [adspsc83x.m33] halted due to debug-request, current mode: Thread xPSR: 0x69000000 pc: 0x000074f8 msp: 0x201ff3bc Info : New GDB Connection: 2, Target adspsc83x.m33, state: halted
Edit Notes
Updated CCES version[edited by: Rob Belcham at 3:20 PM (GMT -5) on 13 Nov 2025]