Post Go back to editing

POST_SC835_SHARCFX_Core1 project does not compile out-of-the-box

Thread Summary

The user encountered build errors in the Power_On_Self_Test_SC835_SHARCFX project due to the adi_xspi library not being correctly set up in CCES 3.0.3. The solution involves removing and reinstalling the xSPI add-in in the system.svc file, then rebuilding the project. This resolves the issue with the xSPI driver configuration for the ADSP-SC83x/ADSP-21568 family of processors.
AI Generated Content
Category: Software
Product Number: 3.0.3
Software Version: 3.0.3

Hi, 
I have installed the ADSP-SC583W SOM board support package and have opened a fresh installation of CCES version 3.0.3. 
I have opened the Power_On_Self_Test_SC835_SHARCFX project from the 'Browse Examples' menu. 
Select the project from the project explorer and build the project. 

Result: 


It appears the adi_xspi library is not correctly setup for the POST build.
How can I resolve this issue?