Hi,
I am using the 21835-SOM development board.but when I running "Flash_Programmer_21835_EZKIT.bat",After a long time, I still cannot complete the download.
Please help me solve this problem.
Regards,
Bingo
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADSP-21835
Recommended for New Designs
The ADSP-2183x/ADSP-SC83x digital signal processors (DSPs)
are members of the SHARC®-FX family of products. The
SHARC-FX core uses a single-instruction...
Datasheet
ADSP-21835 on Analog.com
Hi,
I am using the 21835-SOM development board.but when I running "Flash_Programmer_21835_EZKIT.bat",After a long time, I still cannot complete the download.
Please help me solve this problem.
Regards,
Bingo
Santhakumari - Moved from Processors and DSP to CrossCore Embedded Studio and Add-ins. Post date updated from Friday, September 19, 2025 4:28 AM UTC to Friday, September 19, 2025 6:12 AM UTC to reflect the move.
Hi Bingo,
Thank you for your inquiry.
Using the "Flash_Programmer_SC835_EZKIT.bat" script, we successfully flashed LED Blinking application onto the ADSP-SC835-SOM evaluation board. Please refer the attached screenshot.
To isolate your issue, could you please provide the below details.
1. What kind of application are you attempting to flash onto the ADSP-21835-SOM evaluation board?
2. Please share a screenshot of the command prompt output after executing the "Flash_Programmer_21835_EZKIT.bat" script.
3. Is this issue occurring with all applications, or only with a specific one?
4. Have you tried flashing the application using the CCES IDE instead of using batch script?
5. Can you attempt the flashing process on a different computer and CCES version (3.x.x) to check if the issue still persists?
6. If you have access to another development board and emulator, could you please try flashing the same application there and let us know the outcome?
Thanks in advance and waiting for your reply.
Regards,
Santha kumari.V

Hi,
I can successfully download it using CCES3.0.2,but the BMODE must be set to 0.Is this considered normal?
Please tell me how to use the CCES to flashing LDR?
Regards,
Bingo
Hi Bingo,
Yes, setting BMODE to 0 is required for successfully flashing an LDR file onto the ADSP-SC835-SOM evaluation board using CLDP or the CCES GUI.
For detailed guidance on flashing via the CCES GUI, refer to the "Booting an Application" section available in the CCES Help documentation at the following path:
Help > CrossCore® Embedded Studio 3.x.x > SHARC®-FX Development Tools Documentation > Getting Started Guide > Getting Started Guide for CrossCore Embedded Studio with SHARC-FX support
Note: Make sure your application does not perform any standard I/O functions, such as printf. These functions cannot be used without a debugger attached, and may cause your application to fail to run.
Hope this helps.
Best Regards,
Santha kumari.V
Hi Bingo,
Yes, setting BMODE to 0 is required for successfully flashing an LDR file onto the ADSP-SC835-SOM evaluation board using CLDP or the CCES GUI.
For detailed guidance on flashing via the CCES GUI, refer to the "Booting an Application" section available in the CCES Help documentation at the following path:
Help > CrossCore® Embedded Studio 3.x.x > SHARC®-FX Development Tools Documentation > Getting Started Guide > Getting Started Guide for CrossCore Embedded Studio with SHARC-FX support
Note: Make sure your application does not perform any standard I/O functions, such as printf. These functions cannot be used without a debugger attached, and may cause your application to fail to run.
Hope this helps.
Best Regards,
Santha kumari.V