Post Go back to editing

Error installing CrossCoreEmbeddedStudio-Rel2.12.1

Category: Software
Product Number: CCES
Software Version: 2.12.1

Hi Team,

 I've recently purchased an EVAL-21489-EZLITE board. I am trying to install CCES version 2.12.1 on my Windows 11 home edition OS. However on installation I get the error "Error reading setup initialization file". I right clicked ran as administrator, no avail. Attaching the screenshot, please advice.

Parents
  • Hi,

    It is possible that the installation file that you have is corrupted or the download has not been completed. Sometimes this can happen, if your internet connection is slow or your anti-virus software is scanning the file during the download process.

    So, can you please try to download the file again on a different location on your machine, then check again? as well as temporarily disable your antivirus before downloading the file.

    Also, the actual size of CCES version 2.12.1 is 88,6796 KB. Please check whether the size of CCES version 2.12.1 is 88,6796 KB or different.

    Waiting for your reply.

    Regards,
    Santhakumari.K

  • Hi Santhakumari,

     Yes, the file size is correct. I tried installing on a windows 10 pro edition and it worked. So I've downgraded my OS to from Window 11 home to Windows 10 home edition. I am able to install and use CCES 2.12.1 now.

    Has CCES been tested on Windows 11?

    Regards,

    Rithesh

Reply Children
  • Hi,

    Yes, CCES has been completely tested on Windows 11 and the supporting operating systems are given below

    · Windows 11 Pro or Enterprise (64-bit)

    · Windows 10 Pro or Enterprise (32 and 64-bit)

    · Ubuntu 22.04 (with 32-bit compatibility libraries installed)

    · Ubuntu 20.04 with 32-bit compatibility libraries installed

    Regards,
    Santhakumari.K