ADSP-SC587
Production
The ADSP-SC587 processor is part of the new, high-performance, power-efficient, real-time series that delivers greater than 24 giga-floating-point operations...
Datasheet
ADSP-SC587 on Analog.com
I'm working with CCES 2.7.0, and I need to manually modify the ldf file to adjust the range of some memory segments. This cannot be done using the "Startup Code/LDF" Add-in , nor by inserting anything in $VDSG sections. So I want to use my own custom LDF file.
I'm currently using "Startup Code/LDF" for both startup and ldf files generation. Is there a way to disable LDF generation only? (possibly by modifying the svc file)
Hi,
You can use custom LDF file by renaming that file like "custom.app.ldf" and add to project by browsing into -T switch, which is available by go to Project > Properties > C/C++ Build > Settings > Tools Settings > CrossCore SHARC Linker > General.
-T switch directs the compiler to use the specified linker description file (.ldf) as control input for linking. Try using the below command to add custom_app.ldf
"${ProjDirPath}/system/startup_ldf/custom_app.ldf". If the custom LDF is not specified, then the default LDF for your processor is used.
Hope this helps.
Regards,
Santhakumari.K