Hi.
ADI out the new product ADSP1802. I read datasheet and I think ADSP1802 is low count pin ADSP2148x with L2.
But CCES 3.x.y don't support legacy Sharc. So what kind CCES's version would support ADSP1802?
Best regards.
Hi,
Thank you for your query. We are checking this with our Internal team. We will update to you soon.
Best Regards,
Santhakumari.K
Hi,
Our sincere apologies for the delay in response.
Yes. As you mentioned it is similar to legacy Sharc2148x with additional memory support.
ADSP1802 is supported with CCES 2.11.2 which is a special CCES and yet to be released.
For download this package, please send a mail request to processor.tools.support@analog.com.
Best regards,
Santhakumari.K
Hi,
will the examples for 21479ezkit, like AD1939_Sample_Based_Talkthru_48_Or_96kHz, work on this board?
Regards,
Roman
Hi Roman,
There would be definitely design difference between both boards even though CODECs are same. So you have to port 21479ezkit examples for running it in ADSP-1802 Evaluation kit.
We have a separate BSP package for evaluating ADSP-1802 processor. Please download the package from the below link
www.analog.com/.../eval-adsp1802.html
Hope this helps.
Best Regards,
Santhakumari.K
Hi,
Does the ADSP-1802 support development using SigmaStudio for SHARC platform? What adjustments and changes should be made? Are there examples for reference? I tried to modify the ADSP-21489 DEMO in SigmaStudioForSHARC-SH-Rel2.20, but it didn't succeed in the end. I need your help, thank you.
Hello,
Thank you for your inquiry. Can you please post your query in Sigma Studio for SHARC (SigmaStudio for SHARC) forum.
Best Regards,
Santhakumari.K