Post Go back to editing

Add support for Zephyr OS

Category: Software
Product Number: ADSP-BF527

Since ADI has officially joined the Zephyr Project, Is there any plan from ADI to add support for Zephyr OS to Blackfin Processors (and especially BF527)?

See here

Thread Notes

Parents Reply Children
  • Hi  

    more or less 10 years ago I developed a project based on ADI BF527 using VDK + lwIP.

    The product is in full production at the moment, adding new features, and I don't see any issue from the harware side.

    From the software side, the situation is completely different: VDK + lwIP is an old, outdated and badly supported ecosystem.

    Adding new features (when requested by customers or by the market) is a challenge.

    I've been thinking about how to handle the future of this project:

    • if a well-known vendor-agnostic framework (like Zephyr OS) is going to come into stage in the future, I would consider keeping Blackfin solution
    • if not, I'm going to migrate the project to another architecture (ARM Cortex-M + DSP extension)
  • Thanks for the details! That's very useful.