Since ADI has officially joined the Zephyr Project, Is there any plan from ADI to add support for Zephyr OS to Blackfin Processors (and especially BF527)?
See here
ADSP-BF527
Production
The high performance 16/32-bit Blackfin embedded processor core, the flexible cache architecture, the enhanced DMA subsystem, and the dynamic power management...
Datasheet
ADSP-BF527 on Analog.com
Since ADI has officially joined the Zephyr Project, Is there any plan from ADI to add support for Zephyr OS to Blackfin Processors (and especially BF527)?
See here
Ranji - Moved from Blackfin Processors to CrossCore Embedded Studio and Add-ins. Post date updated from Tuesday, February 20, 2024 2:10 PM UTC to Wednesday, February 21, 2024 9:20 AM UTC to reflect the move.
Hi Vix,
Unfortunately there is no plan to support Zephyr on the Blackfin processors. Can you provide some information about your requirements for us to factor into any future discussions about viability?
Regards,
Murray
Hi MurrayA
more or less 10 years ago I developed a project based on ADI BF527 using VDK + lwIP.
The product is in full production at the moment, adding new features, and I don't see any issue from the harware side.
From the software side, the situation is completely different: VDK + lwIP is an old, outdated and badly supported ecosystem.
Adding new features (when requested by customers or by the market) is a challenge.
I've been thinking about how to handle the future of this project:
Thanks for the details! That's very useful.