| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Awaiting Customer Response | |
I am trying to use the linkport device driver in CCES 2.10.1 to configure a DMA operation using a TCB list. There are 5 TCBs in the list.
I configure the list so that that first 4 TCBs do _not_ request an interrupt when the XCNT is complete, and I configure the last TCB so it _does_ request an interrupt. What I am trying to do is let the DMA handle the entire list without any core involvement and then get a single interrupt when the entire list is complete. I think the hardware supports this style of operation but it appears the device driver requires an interrupt during every TCB.
If I only set the configuration for the last TCB to ENUM_DMA_CFG_XCNT_INT then I get one interrupt the first time I call adi_linkport_DMATransfer(..) but the next time I call the operation does not succeed. If I set ENUM_DMA_CFG_XCNT in every TCB everything works great but an interrupt is generated for every TCB in the list, and I don't need or want that.
My call is adi_linkport_DMATransfer(hDevice, (ADI_PDMA_DESC_LIST*) DescList, 5, ADI_PDMA_DESCRIPTOR_LIST);
Has anyone succeed with using the linkport driver with TCB list where only the last TCB interrupts? Does anyone in ADI know the driver well enough to say if this is possible. I have tried reading the driver code but I may be missing something.
GenevaCooper - Moved from How to Use EngineerZone to SigmaStudio for SHARC. Post date updated from Wednesday, January 24, 2024 6:12 PM UTC to Wednesday, January 24, 2024 8:45 PM UTC to reflect the move.
santha.vijay - Moved from SigmaStudio for SHARC to CrossCore Embedded Studio and Add-ins. Post date updated from Wednesday, January 24, 2024 8:45 PM UTC to Thursday, January 25, 2024 5:38 AM UTC to reflect the move.