Post Go back to editing

Static code analysis with visualDsp++5.0

Hi,

I'm running Klocwork static code analysis for project that built with VisualDsp++,

Build time taken 21 minutes.

When i run static code analysis build time taken 3:30 hours, 

After examination of the debug log provided, i noticed the following process cumulative times in your build (each line represents a process and how long it took in your build in total):
C:\WINDOWS\SysWOW64\cmd.exe 7s
C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\elfloader.exe 15s
C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\linker.exe 33s
C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\TS\etc\ipa.exe 38s
C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\TS\etc\compiler.exe 566s
C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\pp.exe 1805s
C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\TS\etc\prelinker.exe 6999s
C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\easmts.exe 12449s
C:\Program Files (x86)\analog Devices\VisualDSP 5.0\gmake-378.exe 13236s
C:\Program Files (x86)\Analog Devices\VisualDSP 5.0\ccts.exe 20145s

Can i detach some of commands? for decrease build time?

Thanks,

Zion Adadi 

  • Hi,

    Unfortunately , we do not have tested with Klocwork as a code analysis tool in VisualDSP++.

    The recommended products for Static Code Analysis Tools, we can recommend a company called LDRA (http://www.ldra.com). They provides code coverage tools as well as assistance with certification.

    The LDRA tool provides automated software testing and verification of software development and this will be integrated with VDSP++ for use when working with Analog’s embedded processors.

    Additionally, BullseyeCoverage: www.bullseye.com<http://www.bullseye.com> provide code coverage which is compatible with VisualDSP++ 5.x.


    Regards,
    Nishanthi.V