Post Go back to editing

CCES runner can't use custom Platform

Product Number: ADSP-SC572
Software Version: 2.11.0

Hello, I created a platform using CCES debug configurator. The platform is custom. I can launch a debug session with it in CCES, and I can see it listed when I run cces_runner.exe --list. 

However when I use it in the --platform, instead of the default ADSP-SC572 via ICE 1000. It doesn't work.

I basically see nothing happen.

 - No response from the application in the command line

- I don't see the LED on the ICE 1000 change

- I don't see my firmware flashed on the processor. 

Please help