Hello,
I'm working on an own design of ADSP-21569 (nearly identical with the ADSP-21569-SOM). The SPI flash is the same as on the ADZS-21569-EZKIT (IS25LP512M-JLLE).
When I try to program the flash using device programmer in CCES (setup as described here: https://ez.analog.com/dsp/software-and-development-tools/cces/f/q-a/557249/failed-to-execute-the-device-programmer) I get the following error message:
Downloading to device... 'Invoking: CrossCore SHARC Device Programmer' cldp -proc ADSP-21569 -cmd prog -driver "C:\Analog Devices\ADSP-2156x_EZ-KIT-Rel1.0.1\ADSP-2156x_EZ-KIT\Examples\Device_Programmer\Legacy_SPI\is25lp512m_dpia_2156x\21569\is25lp512m_dpia_21569.dxe" -erase affected -emu ice-1000 -format bin -offset 0x0 -file DSP_Firmware.ldr Error: couldn't find DPIA buffer address Error: 13 - Error in Setup Error: driver load failed. Target Emulation Debug Target Platform ADSP-21569 via ICE-1000 Processor ADSP-21569 Core 0 Driver C:\Analog Devices\ADSP-2156x_EZ-KIT-Rel1.0.1\ADSP-2156x_EZ-KIT\Examples\Device_Programmer\Legacy_SPI\is25lp512m_dpia_2156x\21569\is25lp512m_dpia_21569.dxe make: *** [makefile:135: program_device] Error -1 Error during device programming
Related thread to: https://ez.analog.com/dsp/software-and-development-tools/cces/f/q-a/67608/couldn-t-find-dpia-buffer-address-error
Do I need to modify the driver, although I am using the same SPI flash as on the EZ-Kit?
Kind regards,
Markus
Edit Notes
Edited title[edited by: MKrautter at 6:40 AM (GMT -4) on 6 Apr 2023]