Hi ADI experts,
Now I'm developing ANC solution based on the ADC DAC playback SC589 example codes on ADZS-SC584-EZLITE board.
And I have two questions.
1) How could I measure the delay of an external analog loopback (from RCA audio output to RCA audio input) on ADZS-SC584-EZLITE board?
-> Could I estimate the delay using correlation?
2) How could I minimize the delay of an external analog loopback (from RCA audio output to RCA audio input) on ADZS-SC584-EZLITE board?
-> Do I need to modify AUDIO_BUFFER_SIZE to a smaller size in the adc_dac_playback.h file of the ADC DAC playback example?
Thanks for your support!
Kim