Post Go back to editing

Unable to launch debug configuration on CCES

Hello

I am facing launch debug configuration error on CCES. The error is "Failed to Load ADsp Common dll". Although I tried all method available on the forum as clean installation, environment variable set, java fresh installation. Attached is the error. Please look into the matter and guide me on this. 

Thank You

Anukul Anand

Parents
  • Hello,

    We had seen this issue before, if some of the dll file is missing in the CCES installation path.

    Can you please try replacing the attached "cdtarget.dll" , "AdspCommon.dll and "cces.ini" files in the below CCES installation path and restart CCES application. Then try create the session and check if this issue still occurs.
    C:\Analog Devices\CrossCore Embedded Studio 2.9.2\System\

    Before replacing can you please take a backup copy of old "cdtarget.dll", AdspCommon.dll and "cces.ini" files if exists.

    If the problem still appears, can you please try run the CCES 2.9.2 installer using the "Run as Administrator" option, which is available by right-clicking on the *.exe file. Once you have installed with this method please let us know if the behavior still persists.

    Also, can you please check again, since you have already set the environment variable and make sure that it's set to the right installation of CCES? e.g., as you are running CCES 2.9.2, the CCES_HOME environment variable should be set to the CCES 2.9.2 install directory. Please refer attached screenshot for reference(CCES_HOME.JPG).

    If you set the environmental variable CCES_HOME to a directory other than the CCES installation that you're using, then Debug sessions will not operate correctly

    If this issue still occurs,please share us the below details to assist you further

    1. Please let us know which operating system and processor that you are using.

    2. Can you please share us the complete screenshot of your system information.This can be done by pressing Windows+R to open the Run box. Type “msinfo32” into the “Open” field, and then hit Enter. Also,please confirm whether you are using Virtual machine?

    3. Can you please try to debug the project in different PCs and let us know how you get on.

    4. Please let us whether you have installed any antivirus software. If so, please uninstall the antivirus software and then try again.

    Regards,
    Santhakumari.K

    Ezone-547832.rar

  • Hello

    This attached file is corrupted. And the environment variable for 2.9..2 is incorrectly set as 2.9.1. Now the debug configuration is working fine. Thank you for the response. 

Reply Children
No Data