Command Line Device Programmer (cldp) missing Supported processors

ADSP-BF537

CrossCore 2.8.2.0

Custom board

I am attempting to setup a laptop for manufacturing. The laptop will be used to program the BF537 using the cldp program.

I have cldp working on my PC, but when I attempt to use cldp on the laptop cldp's list of supported processors is empty.

C:\Analog Devices\CrossCore Embedded Studio 2.8.2>cldp -proc

Supported processors:

The BF537 EZ-LITE kit is installed on the laptop.

What do I need to do to setup cldp to support the BF537?

Thanks,

BZ

Parents Reply Children