Ethernet On ADSPBF609

Hi All,

I want to work for ethernet driver on Blackfin(BF609). Can we use lwip on Baremetal? or Suggest me how to implement the ethernet driver on BF609 .

Target : ADSP BF609

Tool : CCES

Thanks

bhargavi  

Top Replies

Parents
  • 0
    •  Analog Employees 
    on Jun 17, 2021 10:55 AM

    Hi Bhargavi,

    Yes. You can use LWIP with baremetal framework also.

    Please install the required middleware available in our webpage www.analog.com/.../adswp-lwip.html

    We request you to refer the Ethernet loopback code available in POST example project in the below BSP installation path.

    C:\Analog Devices\ADSP-BF609_Evaluation_Board-Rel1.0.3\BF609_EZ-Board\Blackfin\Examples\Power_On_Self_Test.

    Please go through "readme.html" available in the following path C:\Analog Devices\ADSP-BF609_Evaluation_Board-Rel1.0.3\BF609_EZ-Board\Blackfin\Examples\Power_On_Self_Test for hardware setup before running the loopback code

    Best Regards,
    Santhakumari.K

  • Thanks for your reply Santha. 

    As per your suggestion i installed adsp-lwip then i tried file server example program which is located in below path.

    C:\Analog Devices\lwip_Stack_rel2.6.0/lwip/Blackfin/example/fileserver.

    I gave static IP address. Im changed variable i.e use_dhcp as 1 to 0.In file

    fileserver/system/Lwip/GeneratedSources/lwip_app.c

    After running that program on both sides (server and client side). I got the below error attached with the post.

Reply
  • Thanks for your reply Santha. 

    As per your suggestion i installed adsp-lwip then i tried file server example program which is located in below path.

    C:\Analog Devices\lwip_Stack_rel2.6.0/lwip/Blackfin/example/fileserver.

    I gave static IP address. Im changed variable i.e use_dhcp as 1 to 0.In file

    fileserver/system/Lwip/GeneratedSources/lwip_app.c

    After running that program on both sides (server and client side). I got the below error attached with the post.

Children