How do I find Device Programmer for ADSP-21479 EZKIT when using CrossCore Development ? C:\Analog Devices\CrossCore Embedded Studio 2.9.4\SHARC\Examples\Device_Programmer folder does not list it.
How do I find Device Programmer for ADSP-21479 EZKIT when using CrossCore Development ? C:\Analog Devices\CrossCore Embedded Studio 2.9.4\SHARC\Examples\Device_Programmer folder does not list it.
Hi,
You can find the device programmer examples from the below linked ADSP-21479 EZKIT Board support Package.
http://download.analog.com/tools/EZBoards/21479/Releases/Release_1.0.0/ADI_ADSP-21479_EZKIT-Rel1.0.0.exe
After the successful installation, You can find the example from the below BSP installation path.
<installation path>:\Analog Devices\ADSP-21479_EZKIT-Rel1.0.0\21479_EZ-Board\Examples\Device_Programmer
Regards,
Nishanthi.V
Thank you for sending ADSP-21479 EZKIT BSP. If I need ADSP-21489 EZKIT BSP I could not reach the location ? Why ? And also I have VisualDSP++5.1.2 where there are Flash Programmers (and many examples) for SHARC and Blackfin devices. However CCES only have few examples why ? Where can I download what I need ?
Currently I need ADSP-21489 Parallel Flash Programmer.
Thank you for your support.
Osman
Hi,
You can download ADSP-21489 BSP from the below link:
download.analog.com/.../ADI_ADSP-21489_EZKIT-Rel1.0.0.exe
After installing the BSP successfully,you can get examples in the below path
<Installation path>\Analog Devices\ADSP-21489_EZKIT-Rel1.0.0\21489_EZ-Board\Examples
All the available Board Support Package are provided in the link below:
download.analog.com/.../all_examples.html
Regards,
Nishanthi.V
Dear Nishanthi,
I received both 21479 and 21489 Device Programmer (21489_m29w320_dpia.dxe) that will be used to parallel FLASH programming. I programmed the parallel FLASH (M29W320EB70ZE6E) by using 21479_m29w320_dpia.dxe. It works just fine. Thank you for the help.
One further question is that can I use the same parallel Flash program (21489_m29w320_dpia.dxe) if I make my own PCB circuit board using same parallel FLASH (M29W320EB70ZE6E) ?
Osman
Hi,
Yes, you can use the flash driver available in the BSP for the flash part M29W320EB70ZE6E used in custom board also.
Regards,
Nishanthi.V
Hi,
Yes, you can use the flash driver available in the BSP for the flash part M29W320EB70ZE6E used in custom board also.
Regards,
Nishanthi.V