How do I find Device Programmer for ADSP-21479 EZKIT when using CrossCore Development ? C:\Analog Devices\CrossCore Embedded Studio 2.9.4\SHARC\Examples\Device_Programmer folder does not list it.
How do I find Device Programmer for ADSP-21479 EZKIT when using CrossCore Development ? C:\Analog Devices\CrossCore Embedded Studio 2.9.4\SHARC\Examples\Device_Programmer folder does not list it.
Hi,
You can find the device programmer examples from the below linked ADSP-21479 EZKIT Board support Package.
http://download.analog.com/tools/EZBoards/21479/Releases/Release_1.0.0/ADI_ADSP-21479_EZKIT-Rel1.0.0.exe
After the successful installation, You can find the example from the below BSP installation path.
<installation path>:\Analog Devices\ADSP-21479_EZKIT-Rel1.0.0\21479_EZ-Board\Examples\Device_Programmer
Regards,
Nishanthi.V
Thank you for sending ADSP-21479 EZKIT BSP. If I need ADSP-21489 EZKIT BSP I could not reach the location ? Why ? And also I have VisualDSP++5.1.2 where there are Flash Programmers (and many examples) for SHARC and Blackfin devices. However CCES only have few examples why ? Where can I download what I need ?
Currently I need ADSP-21489 Parallel Flash Programmer.
Thank you for your support.
Osman
Hi,
You can download ADSP-21489 BSP from the below link:
download.analog.com/.../ADI_ADSP-21489_EZKIT-Rel1.0.0.exe
After installing the BSP successfully,you can get examples in the below path
<Installation path>\Analog Devices\ADSP-21489_EZKIT-Rel1.0.0\21489_EZ-Board\Examples
All the available Board Support Package are provided in the link below:
download.analog.com/.../all_examples.html
Regards,
Nishanthi.V
Dear Nishanthi,
I received both 21479 and 21489 Device Programmer (21489_m29w320_dpia.dxe) that will be used to parallel FLASH programming. I programmed the parallel FLASH (M29W320EB70ZE6E) by using 21479_m29w320_dpia.dxe. It works just fine. Thank you for the help.
One further question is that can I use the same parallel Flash program (21489_m29w320_dpia.dxe) if I make my own PCB circuit board using same parallel FLASH (M29W320EB70ZE6E) ?
Osman
Dear Nishanthi,
I received both 21479 and 21489 Device Programmer (21489_m29w320_dpia.dxe) that will be used to parallel FLASH programming. I programmed the parallel FLASH (M29W320EB70ZE6E) by using 21479_m29w320_dpia.dxe. It works just fine. Thank you for the help.
One further question is that can I use the same parallel Flash program (21489_m29w320_dpia.dxe) if I make my own PCB circuit board using same parallel FLASH (M29W320EB70ZE6E) ?
Osman
Hi,
Yes, you can use the flash driver available in the BSP for the flash part M29W320EB70ZE6E used in custom board also.
Regards,
Nishanthi.V