Post Go back to editing

About ADZS-SC584-EZLITE and its User Manual content and ICE-1000 issues

Dear experts,
I have three questions about the ADZS-SC584-EZLITE and ICE-1000 and need your helps.

1. Based on its user manual page 17. It shows that "Attach the emulator header (J2) on the bottom of the ICE-1000 to the P3 connector on the EZ-Board.".
However, the pitch of P3 connector and its circuit content are incorrect to ICE-1000.
I guess the correct connector should be the P1, am I right?
The ADZS-SC584-EZLITE User Manual is here.(www.analog.com/.../adsp-sc584-ezboard-manual.pdf)


2. The extending issue from 1st question, if the Debug COM is P1(in EVB), I think it is not robust for their connecting way via J2 of emulator header.
I prefer to use the extention cable(from ICE-1000) for jumping wires to connect to P1(in EVB).
The ICE-1000 User Manual is here.(www.analog.com/.../ICE_emu_1000_2000_rev_manual.pdf)
But I can't get this cable circuit from the ADI website.
So I don't know the pin definition of output header of this cable.
Where can I get this circuit?
Can I directly insert this cable(from ICE-1000) into the P1 connector(in EVB) for downloading the FW or debugging?


3. Based on its user manual page 17. It shows that "Attach the provided cord and appropriate plug to the 5V power adaptor.".
However, the adopt attached by the ADZS-SC584-EZLITE box is 12V.
Which power level is correct? 5V or 12V?
Can I apply the 12V adaptor on this EVB?

Please help me and thanks for your helps.



robest -> robust
[edited by: s909201@gmail.com at 6:09 AM (GMT -4) on 15 Mar 2021]