ConfigSoftSwitches() question

Hello!

I want to ask a question about ConfigSoftSwitches() function.

I'm using a custom board with ADSP BF-609 processor.  You may find ConfigSoftSwitches() function in  lwip_sysboot_task() when you add lwip add-in to the project.

ConfigSoftSwitches() operates with array of structures SOFT_SWITCH types. Each SOFT_SWITCH cell contains field HardwareAddress and this values hardcoded for each cell. In my case this is 0x21, 0x22, 0x23, see code below.

static SOFT_SWITCH SoftSwitch[] =
{
  {
    0u,
    0x21u,
    sizeof(SwitchConfig0)/sizeof(SWITCH_CONFIG),
    SwitchConfig0
  },
  {
    0u,
    0x22u,
    sizeof(SwitchConfig1)/sizeof(SWITCH_CONFIG),
    SwitchConfig1
  },
#if defined(__ADSPBF609__)
  {
    0u,
    0x23u,
    sizeof(SwitchConfig2)/sizeof(SWITCH_CONFIG),
    SwitchConfig2
  },
#endif
};

My first question is why this thing uses 0x21, 0x22, 0x23 values? Is there anywhere information about this hardware addresses and matches with hardware that was be used on the board?

I didn't find information about this moment in hardware references.

Also each SoftSwitch[0], SoftSwitch[1], SoftSwitch[2] contains field SwitchConfig0, SwitchConfig1, SwitchConfig2 correspondingly.

For SwitchConfigs I can see next definitions:

static SWITCH_CONFIG SwitchConfig0[] =
{
/*
            U45 Port A                                  U45 Port B

    7--------------- RMII_CLK_EN        |       7--------------- ~TEMP_THERM_EN
    | 6------------- ~CNT0ZM_EN         |       | 6------------- ~TEMP_IRQ_EN
    | | 5----------- ~CNT0DG_EN         |       | | 5----------- ~UART0CTS_146_EN
    | | | 4--------- ~CNT0UD_EN         |       | | | 4--------- ~UART0CTS_RST_EN
    | | | | 3------- ~CAN0RX_EN         |       | | | | 3------- ~UART0CTS_RTS_LPBK
    | | | | | 2----- ~CAN0_ERR_EN       |       | | | | | 2----- ~UART0CTS_EN
    | | | | | | 1--- ~CAN_STB           |       | | | | | | 1--- ~UART0RX_EN
    | | | | | | | 0- CAN_EN             |       | | | | | | | 0- ~UART0RTS_EN
    | | | | | | | |                     |       | | | | | | | |
    N Y Y Y Y N N Y                     |       N N N N N N Y Y     ( Active Y or N )
    1 0 0 0 0 1 1 1                     |       1 1 1 1 1 1 0 0     ( value being set )
*/

  { 0x12u, 0x87u },                          { 0x13u, 0xFCu },

  /* specify inputs/outputs */
  { 0x0u, 0x0u },
  { 0x1u, 0x0u },
};
/* switch 1 register settings */
static SWITCH_CONFIG SwitchConfig1[] =
{
/*
            U46 Port A                                  U46 Port B

    7--------------- ~LED4_GPIO_EN          |       7--------------- EMPTY
    | 6------------- ~LED3_GPIO_EN          |       | 6------------- ~SPI0D3_EN
    | | 5----------- ~LED2_GPIO_EN          |       | | 5----------- ~SPI0D2_EN
    | | | 4--------- ~LED1_GPIO_EN          |       | | | 4--------- ~SPIFLASH_CS_EN
    | | | | 3------- SMC0_LP0_EN            |       | | | | 3------- ~SD_WP_EN
    | | | | | 2----- EMPTY                  |       | | | | | 2----- ~SD_CD_EN
    | | | | | | 1--- SMC0_EPPI2_LP1_SWITCH  |       | | | | | | 1--- ~PUSHBUTTON2_EN
    | | | | | | | 0- OVERRIDE_SMC0_LP0_BOOT |       | | | | | | | 0- ~PUSHBUTTON1_EN
    | | | | | | | |                         |       | | | | | | | |
    Y Y Y Y Y X Y Y                         |       X Y Y Y Y Y Y Y     ( Active Y or N )
    0 0 0 0 1 X 1 0                         |       X 0 0 0 0 0 0 0     ( value being set )
*/
  { 0x12u, 0xAu },                                  { 0x13u, 0x0u },

  /* specify inputs/outputs */
  { 0x0u, 0x0u },
  { 0x1u, 0x0u },
};
/* switch 2 register settings */
static SWITCH_CONFIG SwitchConfig2[] =
{
/*
            U47 Port A                                                  U47 Port B

    7--------------- ~PD2_SPI0MISO_EI3_EN                   |       7--------------- EMPTY
    | 6------------- ~PD1_SPI0D3_EPPI1D17_SPI0SEL2_EI3_EN   |       | 6------------- EMPTY
    | | 5----------- ~PD0_SPI0D2_EPPI1D16_SPI0SEL3_EI3_EN   |       | | 5----------- EMPTY
    | | | 4--------- ~WAKE_PUSHBUTTON_EN                    |       | | | 4--------- EMPTY
    | | | | 3------- ~ETHERNET_EN                           |       | | | | 3------- EMPTY
    | | | | | 2----- PHYAD0                                 |       | | | | | 2----- EMPTY
    | | | | | | 1--- PHY_PWR_DWN_INT                        |       | | | | | | 1--- ~PD4_SPI0CK_EI3_EN
    | | | | | | | 0- ~PHYINT_EN                             |       | | | | | | | 0- ~PD3_SPI0MOSI_EI3_EN
    | | | | | | | |                                         |       | | | | | | | |
    N N N N Y N N Y                                         |       X X X X X X N N     ( Active Y or N )
    1 1 1 1 0 0 0 0                                         |       X X X X X X 1 1     ( value being set )
*/
 { 0x12u, 0xF0u },                                                 { 0x13u, 0x3u },

 /* specify inputs/outputs */
  { 0x0u, 0x6u },
  { 0x1u, 0x0u },
};

Structure SWITCH_CONFIG contains fields Register and Value. My second question is why here are used only  0x0u, 0x1u, 0x12u, 0x13u values for Register fields and which number matches with real register name (for example, pREG_DMA33_CFG or maybe another name)? Maybe there is table with coincidence such values and registers names and registers description.

Thanks!

Parents
  • There are four parts to this mystery.  The first is which of the TWI busses is being used.  This is the zero you see at the front of the SoftSwitch[] array (other devkits have a different design and also use TWI1).  The second is the address of the softswitch on the TWI bus.  This is the 0x21, 0x22, and 0x23 values.  If you look at the schematic and locate the TWI0 bus, it will lead you to a general purpose I/O chip, and you can find the datasheet for this part online.  You'll also see how the addresses of these chips are set, and that by giving them different addresses, you can have multiple chips on one TWI bus.  The third mystery is the register address within the softswitch, and this is the first number in the pairs in the SWITCH_CONFIG array (0x12, 0x13, 0x0, 0x1).  Finally, there is the data to be stored at that address, which is the second number in the pair.  You can find more info about what these registers do in the datasheet.

    One thing I haven't figured out is what the comment "Active Y or N" means, or why the values for it aren't limited to Y or N, but also include X.

Reply
  • There are four parts to this mystery.  The first is which of the TWI busses is being used.  This is the zero you see at the front of the SoftSwitch[] array (other devkits have a different design and also use TWI1).  The second is the address of the softswitch on the TWI bus.  This is the 0x21, 0x22, and 0x23 values.  If you look at the schematic and locate the TWI0 bus, it will lead you to a general purpose I/O chip, and you can find the datasheet for this part online.  You'll also see how the addresses of these chips are set, and that by giving them different addresses, you can have multiple chips on one TWI bus.  The third mystery is the register address within the softswitch, and this is the first number in the pairs in the SWITCH_CONFIG array (0x12, 0x13, 0x0, 0x1).  Finally, there is the data to be stored at that address, which is the second number in the pair.  You can find more info about what these registers do in the datasheet.

    One thing I haven't figured out is what the comment "Active Y or N" means, or why the values for it aren't limited to Y or N, but also include X.

Children