Post Go back to editing

Regarding CrossCore Embedded Studio (CCES) IDE development licenses

Thread Summary

The ADSP-BF609 EZ Kit Lite does not include a CCES license. A free 90-day evaluation license is available upon first run of CrossCore Embedded Studio. For custom board development, an Evaluation or Full license is required, as custom targets are not supported by the EZ-Kit license.
AI Generated Content

Hello,

Need to know if we buy "ADSP-BF609 EZ Kit Lite" will we get the IDE Licenses along with the eval kit.  

Later if we need to develop the code for the custom board based on the same BF609 processor, can we used the same license for development. Are there any restrictions?

-Regards 

  • Hi,

    1. Need to know if we buy "ADSP-BF609 EZ Kit Lite" will we get the IDE Licenses along with the eval kit.
    >> The ADSP-BF609 EZ Kit Lite package does not come with a separate CCES License.

    An EZ-KIT license is included with EZ-KIT evaluation boards for the following parts only: ADSP-21569, ADSP-BF706, ADSP-BF707, ADSP-SC573, ADSP-SC584, ADSP-SC589 and ADuCM3029

    Instead, CrossCore Embedded Studio comes with a free Evaluation license built in which, once activated, will allow you full access to the tools for a 90 day period.

    ADSP-BF609 EZ-Kits require an Evaluation or Full license to use CrossCore Embedded Studio.

    An evaluation license can be obtained from CrossCore Embedded Studio,which offers a tool chain evaluation license the first time it runs. It can be activated once on a particular machine. Once entered and activated, the license will be valid for 90 days.

    You can refer the below FAQ for more details:
    FAQ: How can I obtain and install a licenses for CrossCore Embedded Studio?
    ez.analog.com/.../faq-how-can-i-obtain-and-install-a-licenses-for-crosscore-embedded-studio

    You can also buy a full license for CCES, using the below link:
    www.analog.com/.../adswt-cces.html

    For more details on pricing and discount, please contact your local ADI sales office or distributor.To locate the one,
    www.analog.com/adi-sales

    2. Later if we need to develop the code for the custom board based on the same BF609 processor, can we used the same license for development. Are there any restrictions?
    >>You have to use Evaluation license or Full license for developing the code using custom board. The custom targets are not supported by an EZ-Kit license.

    Regards,
    Nishanthi.V

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.