Post Go back to editing

Add existing source code files to a CCES project that was imported from VDSP

Thread Summary

The user needed to add source code files to a project in CCES without placing them in a subdirectory. The solution involved using the 'New > File from Template' option, enabling 'Link to file in the file system', and browsing to the desired files. The user confirmed this method worked successfully.
AI Generated Content

Hi all,

I migrated a project from VDSP to CCES and now need to add 2 files with source code.

The project structure after that is

+ MyProj

    + MyProj (created by import wizard)

     <all source and header files, etc>

I would like the new files to be in the same folder as the already existing files (and not in the subdirectory created by the import wizard).

I didn't find the right way to do it at first and ended up using "import" -> "file system" which seems to work in principle, but puts the files in the subfolder created by the VDSP import wizard (which contains the system folder).

Manually copying the files in the desired folder and initiating a "Refresh" of the Project Explorer did not work.

Is there any way to achieve this?

Best regards,

Rainer

Parents
  • Hi Rainer,

    Could you please follow the below steps to add existing source code files to a CCES project:

    1. Right click the folder in the project at where you have to place the source files.
    2. Choose New > File from Template.
        The New File wizard appears.
    3. Click Advanced.
    4. Enable Link to file in the file system.
    5. Click Browse and select the file to link.
    6. Click Finish.
        The linked resource appears immediately in the navigation view.

    Please refer in CCES help for more information:

    CrossCore® Embedded Studio 2.x.x > Integrated Development Environment > Managing CCES Projects > Managing Resources> Creating a Linked Resource

    If you are facing any issues, please share us the project along with source files that needs to add.This will help us to assist you further.

    Regards,
    Nishanthi.V

  • Hi Nishanthi,

    that worked flawlessly. Thanks for your quick response!

    Best regards,

    Rainer

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.