CCES Debugger doesn't build all projects before running target

While in CCES 2.8.3 (for Windows) debugger & my target's SHARC Core2 is suspended, I make a change to a source file in my SHARC_Core2 project, stop the debugger with the red square tool "Terminate"), start the debugger with the bug tool "Debug" again. The debugger asks me if I want to save the SHAR_Core2 project's source file I just changed, I click Save, and the CDT Global Build Console window shows it attempts to make my ARM_Core0 project, but none of my other 3 projects:

09:10:43 **** Incremental Build of configuration Debug for project ARM_Core0 ****
make all 
make: Nothing to be done for `all'.

09:10:44 Build Finished (took 441ms)

It used to attempt to make all 4 of my projects, now it doesn't. I tried deleting my SHARC_Core2 project from the SHARC_Core2 project's C/C++ Build Setting's Refresh Policy tab & re-adding it, but it doesn't prevent this problem from happening. I have go to the C/C++ perspective, select all my projects, and click the hammer tool "Build" to get it to make my changed file, as shown in the same CDT Global Build Console window:

09:19:49 **** Incremental Build of configuration Debug for project ARM_Core0 ****
make all 
make: Nothing to be done for `all'.

09:19:49 Build Finished (took 436ms)

09:19:51 **** Incremental Build of configuration Debug for project ABC_Lib ****
make all 
make: Nothing to be done for `all'.

09:19:51 Build Finished (took 229ms)

09:19:54 **** Incremental Build of configuration Debug for project SHARC_Core1 ****
make all 
'Building target: SHARC_Core1.ldr'
'Invoking: CrossCore SHARC Loader'
elfloader -proc ADSP-SC573 -si-revision 0.0 -bspimaster -fbinary -width 8 -bcode 1 -core1="SHARC_Core1.dxe" -MaxBlockSize 2048 -o "SHARC_Core1.ldr"
'Finished building target: SHARC_Core1.ldr'
' '

09:19:55 Build Finished (took 1s.59ms)

09:19:58 **** Incremental Build of configuration Debug for project SHARC_Core2 ****
make all 
'Building file: ../XYZ.cpp'
'Invoking: CrossCore SHARC C/C++ Compiler'
cc21k -c -file-attr ProjectName="SHARC_Core2" -proc ADSP-SC573 -flags-compiler --no_wrap_diagnostics -si-revision 0.0 -g -DCORE2 -DAPP_AVD -DDEBUG -D_DEBUG -DADI_MCAPI @includes-381bbf68305fb13926075ac6a2853044.txt -structs-do-not-overlap -no-const-strings -no-multiline -c++11 -warn-protos -double-size-32 -char-size-8 -swc -gnu-style-dependencies -MD -Mo "XYZ.d" -c++ -o "XYZ.doj" "../XYZ.cpp"
'Finished building: ../XYZ.cpp'
' '
'Building target: SHARC_Core2.dxe'
'Invoking: CrossCore SHARC Linker'
cc21k -proc ADSP-SC573 -si-revision 0.0 -TC:/Users/.../SHARC_Core2/system/startup_ldf/app.ldf -no-mem -LC:/Users/.../SHARC_Core2/Debug/system/startup_ldf -flags-link -MDCORE2,-MDOTHERCORE,-MDDEBUG -add-debug-libpaths -o SHARC_Core2.dxe @input-file.txt  -flags-link -od,.\.
'Finished building target: SHARC_Core2.dxe'
' '

09:20:07 Build Finished (took 8s.928ms)