Apply Master/Slave MDMA from EE377 to ARM/SHARC MDMA

Hi!

I am trying to use the master/slave code from the EE377 to establish the same way of communication between the ARM and one Sharc Core (Sharc Core 1).

But I can't find any correspondig L1 address and the code is not compileable because some defines are not available with the ARM Core (#include <services/int/adi_sec.h>)

Is it even possible to do it that way?

Or do i have to find a total different solution?

Best Regards

Christof