Can't get data ADC data to be in [-1, 1) range on EZ-KIT SC589

Hi all, 

I am having a fight with the SC589 EZ-KIT. 

I am trying to process audio on the floating point domain but I can't get the incoming data from the ADC to be ranged between [-1, 1) as one would expect. 

This is what I'm doing to covert the integer samples from the ADC into a float buffer:

inBufferSplitMono [ i ] = __builtin_conv_RtoF(inSample[ NUM_CHANNELS*i ]);

But then, when plotting that buffer this is what I get for a 0.65Vpeak 1KHz sine tone:

As can be seen there, values are very little. So, I went all the way down to verifying that the samples coming from the ADC (ADAU1977) are correct and found that things are a bit strange down there. This is what the DMA'd memory region looks like:

I'm not sure why the 4th byte is 0xFF for the third channel. 

So, is there anything obvious that I am missing here?

Looking forward to hearing from you.

Thanks in advance!

Manuel

Parents
  • 0
    •  Analog Employees 
    on Mar 22, 2019 2:59 PM over 1 year ago

    Hello,

    We have taken SC-589 audio talk through example and observed similar kind of results.

    In I2S mode, adi_sport_ConfigData() API word width has been set as 24bit. While analyzing the ADC data, the MSB bytes are filled with extended sign byte.

    When we change the word width from 23u to 31u in adi_adau1979.c at line:409, we observed that the extended sign byte has been shifted out and we are getting better floating point data after applying built in fix to fractional conversion function.

    We have given 4k sine tone with 0dB as input and set the volume as maximum and observed that these signed byte has been shifted out.

    Could you please change the configuration and let us know how you are getting on.

    If you still facing issues, please share us the sample project. That will help us assist you better.

    Best regards,
    Santha kumari.K

  • Hi Santha, 

    thank you very much for your quick reply. 

    I have been able to fix the issue by removing the DC offset of the samples by writing 0x0F to ADI_ADAU1979_REG_DC_HPF_CAL. 

    I also multiplied and divide the samples by 256 in order to covert from 24 to 32-bit while keeping the sign bit:

    inBufferSplitMono [ i ] = __builtin_conv_RtoF(inSample[ NUM_CHANNELS*i ] * 256);
    .
    .
    .
    *outSample++ = __builtin_conv_FtoR(inBufferSplitMono[ (0 * numSamples) + i ]) / 256;

    Let me know if something doesn't make sense to you. 

    Manuel

  • 0
    •  Analog Employees 
    on Mar 26, 2019 3:20 PM over 1 year ago in reply to nuel1986

    Hello Manuel,

    We have tried your steps. But we are getting the values in the range of -0.15 to 0.15. We are curious to know whether you are getting the fractional values is in the range of -1 to +1. 

    Best regards,

    Santha kumari.K

  • Hi Santha,

    I have also had to increase the front-end gain by doing this in the Adau1979Init() function: 

    	if((uint32_t)adi_adau1979_SetVolume(phAdau1979, ADI_ADAU1979_AUDIO_CHANNEL1, 128) != 0u)
    	{
    		printf ("ADAU1979: adi_adau1979_RegisterCallback failed\n");
    		/* return error */
    		return 1u;
    	}
    
    	if((uint32_t)adi_adau1979_SetVolume(phAdau1979, ADI_ADAU1979_AUDIO_CHANNEL2, 128) != 0u)
    	{
    		printf ("ADAU1979: adi_adau1979_RegisterCallback failed\n");
    		/* return error */
    		return 1u;
    	}
    
    	if((uint32_t)adi_adau1979_SetVolume(phAdau1979, ADI_ADAU1979_AUDIO_CHANNEL3, 128) != 0u)
    	{
    		printf ("ADAU1979: adi_adau1979_RegisterCallback failed\n");
    		/* return error */
    		return 1u;
    	}
    
    	if((uint32_t)adi_adau1979_SetVolume(phAdau1979, ADI_ADAU1979_AUDIO_CHANNEL4, 128) != 0u)
    	{
    		printf ("ADAU1979: adi_adau1979_RegisterCallback failed\n");
    		/* return error */
    		return 1u;
    	}
    

    Let me know if you need further information. 

    Regards. 

    Manuel

  • 0
    •  Analog Employees 
    on Mar 26, 2019 4:05 PM over 1 year ago in reply to nuel1986

    Hello Manuel,

    Thank you so much for your reply. Hope you are also splitting the incoming Source ADC data into L1,R1,L2,R2 channels. I have tried this step also. But this will increase the noise level when we are not passing any audio input. Have you verified this step.

    Best regards,

    Santha kumari.K

  • hello,where can I find the example about split the incoming source ADC data into L1,R1 L2 R2? thanks

Reply Children
  • 0
    •  Analog Employees 
    on Nov 13, 2019 10:27 AM 11 months ago in reply to jie070428

    Hello,

    Please find the attached Example Audio playback project for SC-589 ezkit which de-interleave the received channel data from ADC 0, 1, 2, 3 into four buffers. Kindly check the de-interleaved from the attached image

    In this example project, we are using ADAU1979 ADC and ADAU1962A DAC

    Here we are converted the source data from real to float if you want to process the data further for example applying filtering logic and in destination buffer we are converted it back to real

    Best Regards,
    Santha kumari.K

    ADC DAC Audio Playback (SC589 SHARC).zip

  • Thank you very much! It help me a lot . I hava some doubt, for this AUDIO_BUFFER_SIZE/(NUM_CHANNELS*4u), I understand that 4u  is 4 byte, 

    now, I want to modify

     /* Macro to set buffer size */
    #define AUDIO_BUFFER_SIZE (SAMPLES_PER_PERIOD * NUM_CHANNELS * SAMPLE_SIZE * 4u)

    to 
    #define AUDIO_BUFFER_SIZE (1u * NUM_CHANNELS * SAMPLE_SIZE ), because I need the  four buffers length is one . dose it fit?  I think  minimal buffer  can be set one, but it dose not have output for ADC 0 1 2 3 

  • 0
    •  Analog Employees 
    on Nov 18, 2019 5:54 AM 11 months ago in reply to jie070428

    Hello,

    Please note that ADC Output Data Bit Width is configured for 24-bit and the SPORT data width is configured for 32-bit (4Bytes). Each ADC channel data size is 32-bit (4-Bytes) in received SPORT buffer. If you are trying to store 32-bit data into 8-bit buffer, remaining bits will be truncated (if you declared *pSrc in 32-bit).

    If this is not your requirement, please explain in detail and share us the code. This will be helpful for us to assist you better.

    Regards,
    Santha kumari.K

  • hello, thanks.  I add FIR filter to ADC DAC PLACKBACK, the filter only work once.  I look the example project: low pass filter  , I see the filter only work once,if I want FIR filter work contiue in ADC_DAC PLACKBACK, could you give me some advince ?thanks

  • 0
    •  Analog Employees 
    on Nov 26, 2019 9:01 AM 10 months ago in reply to jie070428

    Hello,

    Could you please let us know where did you apply your filtering logic?

    Please write your logic in a function and call it after splitting the source data to four channel buffers. After completing this process convert the individual data from float to real and store it in a destination buffer.

    Please refer the below help path which contains information about run-time library functions

    CrossCore® Embedded Studio> SHARC® Development Tools Documentation > C/C++ Library Manual for SHARC® Processors > DSP Run-Time Library > DSP Run-Time Library Reference > fir

    If this is not helpful, please share us the project that you have tried.

    This will be helpful for us to assist you further.
     
    Best Regards,
    Santha kumari.K