Article How to use commands in CCES runner Audit

How to use ‘--breakpoint’, ‘—datafile’ and ‘-@/ --config’ command with CCES_Runner.exe command line utility

Question:

  1. Is ‘--breakpoint’ command used together with ‘--datafile’ command to rd/wt memory?

Answer:

Yes. The “--breakpoint" option is used in conjunction with the “--datafile" option to read or write memory. For example, to read an array of values to the “output.txt” file from the const variable “values” after halting at a label “breakpt”:

For example:

CCES_runner.exe --target "Emulation Debug Target" --platform "ADSP-21569 via ICE-1000" --processor "ADSP-21569" --core "0, EMU|ANY|CLEAR_SYMBOLS|RUN_AFTER_LOAD|SHARC/ldr/ezkit21569_preload.dxe,21569/Debug/21569.dxe" --datafile "0,out,output.txt,binary,values,40,1,breakpt" --breakpoint "0,breakpt"

Question:

Can ‘—datafile’ command also be used to rd/wt IOP registers?

Answer:

Yes, “--datafile" command can be used to read or write the IOP registers directly. But we can also read the register values via code and store them in a variable to then read via “--datafile".

Question:

Are there any file location demands of configuration file when ‘-@/ --config’ command used?

Answer:

The config file can be located anywhere and either a full path or a path relative to the current working directory must be used.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.