Article What is the purpose of using non-blocking peek functions? Audit

Question:

What is the purpose of using non-blocking peek functions?

Answer:

adi_xxx_IsRxBufferAvailable & adi_xxx_IsTxBufferAvailable APIs are called as non-blocking peek functions and can be used to check if a free buffer is available without blocking. These functions can be used especially in the non-RTOS case to avoid blocking when the buffer is not available.

These APIs are valid for non-blocking mode only.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.