Article Does CrossCore Embedded Studio Support C++ 11?


Question

Does CrossCore Embedded Studio support C++11? If so, what is supported?

-----------------------------

 

Answer:

The Blackfin compiler accepts many features of the ANSI/ISO 14882:2011 Standard (C++11), when the -c++11 switch is used. Note that the underlying run-time library conforms to ANSI/ISO 14882:2003. When the -c++ switch is used, the compiler conforms to the ANSI/ISO 14882:2003 Standard.

The -g++ switch may be used with the Blackfin compiler. It directs the compiler to support many of the GNU G++ extensions to the C++ language. The -g++ switch may be used in conjunction with either the -c++ or -c++11 switches.

These language conformance enhancements are only available in the Blackfin compiler. They are not available in the SHARC compiler.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.