Article Does DDR SDRAM memory reserved for SHARC1 can be used for SHARC0 itself?

Question:

Does SDRAM memory reserved for SHARC1 DDR-A part7 is usable in SHARC0 itself? Is it possible to use both DDR-A part6(112MB) & DDR-A part7 (128MB) memory for SHARC0/Core1 itself?

The DDR SDRAM memory partitions as follows in ldf file:
256MB DMC0 DDR SDRAM memory is partioned as follows:
DDR-A part1 : SHARC0 NW code, 3MB
DDR-A part2 : SHARC1 NW code, 3MB
DDR-A part3 : SHARC0 data, 4MB
DDR-A part4 : SHARC0 VISA code, 3MB
DDR-A part5 : SHARC1 VISA code, 3MB
DDR-A part6 : SHARC0 data, 112MB
DDR-A part7 : SHARC1 data, 128MB

Answer:

Yes. Memory can be re-partitioned as per the need.

However, since this involves parts of the generated LDF that are not enclosed in $VDSG tags used to mark user-modifiable chunks, any changes to them are liable to be overwritten by the Startup/LDF add-in.

Therefore we’d suggest the following process to switch to a custom LDF

Configure the LDF as closely to as per need as the add-in allows and save the settings.
Move the generated app.ldf file from the system/startup_ldf folder to the src folder of project.
Remove the Startup/LDF add-in from the system.svc.
Point the ‘Custom LDF’ setting in the on the Linker/General page of the tool settings at the moved LDF.
Start editing the LDF.

Also ensure that the memory ranges assigned to core 1 and 2 do not overlap. There is no error checking for this so overlaps would likely result in unexpected behaviour at runtime.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.