Article How can I create a copy of example project available in CCES/BSP into the workspace instead of importing example project directly from installation path?

Question:

How can I create a copy of example project available in CCES/BSP into the workspace instead of importing example project directly from installation path?

Answer:

We can create a copy of workspace project into workspace through the Example Browser. So that a copy of the project is physically added to the workspace.

Please follow the below procedure to import example project through the Example Browser:

1.Please open the CCES in the new workspace.

2.To access the Browse Examples page, do one of the following:
•Choose Help > Browse Examples.
•Click Browse Examples from the Welcome page.

3.Choose Type(example project),Product, Family, Processor, Platform and Languages in "Filter examples by" area and Click Search

4.Open a search result. Do one of the following(refer the screenshot):  
   ◦Double-click any result.
   ◦Select an example project and click Open Example.
(When an example is selected, adds the project to the workspace and opens the main code file in the editor area.)

5. Clean and build the project.

Note:
The IDE cannot open the selected project if a project with the same name already exists in the workspace.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.