Article Using CrossCore Embedded Studio's CCES Runner Utility Audit

Overview

This document explains how to load and run programs from the command line using CCES Runner. CCES Runner is a command line utility that can be used to help automate tests. For example, ADI's CrossCore Embedded Studio (CCES) Compiler team runs a suite of automated tests that builds their compiler test programs and then uses CCES runner to run those programs on a target to verify the test results.

Getting Started

Installing CCES Runner from within CrossCore Embedded Studio (CCES)

Installation

  1. From the Help menu, click "Install New Software…".
  2. In the "Work with:" textbox, enter the URL http://www.analog.com/static/ccesupdatesite and hit "Enter".
  3. In the generated list below expand "CrossCore Embedded Studio Command Line Utilities" and choose "CCES Runner".
  4. Click the "Next" button and then the "Next" button again.
  5. Select "I accept the terms of the license agreement" and click "Finish".
  6. Click "Yes" for the restart.

Figure 1: Installing CCES Runner

Updating

  1. To update to the latest version of CCES Runner, under the "Help" menu, click "Check for Updates". If any updates are available they will be installed automatically.

Figure 2: Updating CCES Runner

Or by visiting the "Help" menu, choosing About CrossCore Embedded Studio, Installation Details, click on the feature that you would like to update, and choose "Update...". If any updates are available they will be installed automatically.

Uninstalling

  1. Under the "Help" menu, click "About CrossCore Embedded Studio". Click the "Installation Details" button in this window.
  2. Under the "Installed Software", select CCES Runner and then the "Uninstall…" button at the bottom.
  3. Follow any subsequent prompts and click "Yes" to restart the IDE at the end.

Figure 3: Uninstalling CCES Runner


Running CCES Runner

Once CCES Runner has been installed, the Runner executable file, CCES_runner.exe, will be located under the CrossCore Embedded Studio (CCES) directory. CCES Runner can be run from any directory but if run outside the CCES home directory, the command option --cceshome must be used to specify the location of CCES.

To run CCES Runner:

  1. Open up Command Prompt and navigate to the location of CCES_runner.exe.
  2. Type "CCES_runner.exe" followed by the command line options and arguments.

Example:

To display the help text containing all valid options and their arguments:

Figure 4: Example --help command

Loading and Running Programs

Loading Programs

To run a program, at least these four options must be specified: processor, target, platform, and core. To find the values of these options, the --list option (optional combine with --processor) can be used to list all the possible target and platform values to pass as arguments. Or you can also create a launch configuration in CCES IDE and copy the session configurations into the corresponding command.

Figure 5: Launch configuration in CCES IDE


The following is a brief explanation of the purpose of each command:lo

 

Command

Description

Example

processor The session’s processor. This command must be followed by a string specifying the processor. --processor "ADSP-SC589"
target The session’s target. This command must be followed by a string specifying the target. --target "Emulation Debug Target"
platform The session’s platform. This command must be followed by a string specifying the platform. --platform "ADSP-SC589 via ICE-2000"
core The core as well as its prerequisites (programs that initialize memory and/or set up the system) and program to load and run. The core ID, prerequisites, and program must be separated by a comma. The prerequisite options and program must be separated by a vertical bar, “|”.

--core "0,EMU|KIT|CLEAR_SYMBOLS|RUN_AFTER_LOAD|SHARC\ldr\ezkitSC589_preload_core0_v01,C:\ workspace\ADSP-SC589_Core0\Debug\ADSP-SC589_Core0"

List Command

Use the –list option to view all available targets and platforms. Specify the optional processor string to view all available targets and platforms for a specific processor. The results can then be passed to the --target and --platform commands.

Example:

To list all available combination of targets and platforms for ADSP-BF707:

Figure 6: Example --list command

$ CCES_runner.exe --list --processor ADSP-BF707

Target: ChipFactory Simulator
Platform: ADSP-BF707 Functional-Sim

Target: Blackfin CS Emulator
Platform: ADSP-BF707 via ICE-2000

Target: Blackfin CS Emulator
Platform: ADSP-BF707 via ICE-1000

 

Example command lines to run ADSP-SC589 program(s)

ADSP-SC589 using ICE-2000

$ CCES_runner.exe \
  --target "Emulation Debug Target" \
  --platform "ADSP-SC589 via ICE-2000" \
  --processor ADSP-SC589 \
  --core "0,C:\Users\workspace\cces\2.7.0\test_Core0\Debug\test_Core0" \
  --core "1,C:\Users\workspace\cces\2.7.0\test_Core1\Debug\test_Core1.dxe" \
  --core "2,C:\Users\workspace\cces\2.7.0\test_Core2\Debug\test_Core2.dxe"

ADSP-SC589 using Functional Simulator

$ CCES_runner.exe \ 
--target "ChipFactory Simulator" \ 
--platform "ADSP-SC589 Functional-Sim" \ 
--processor ADSP-SC589 \ 
--core "1,C:\Users\workspace\cces\2.7.0\test_Core1\Debug\test_Core1.dxe" \ 
--core "2,C:\Users\workspace\cces\2.7.0\test_Core2\Debug\test_Core2.dxe"

ADSP-SC589 using Cycle-Accurate Simulator

Please note core id starts from zero.

$ CCES_runner.exe \
  --target "ChipFactory Simulator" \
  --platform "ADSP-SC589 Cycle-Accurate-Sim" \
  --processor ADSP-SC589 \
  --core "0,C:\Users\workspace\cces\2.7.0\test_Core1\Debug\test_Core1.dxe"

Load Prerequisites

As mentioned in the description of the core command, load prerequisites can be specified to be loaded prior to loading the user program. A load prerequisite consists of a DXE file and possible options for that session. Below is a table containing available load prerequisite options:

Options

 

Option

Description

SIM The prerequisite is valid only when connected to a simulator session
EMU The prerequisite is valid only when connected to an emulator session
KIT The prerequisite is valid only when connected to an EZ-KIT Lite session
ANY The prerequisite is valid when connected to any type of session
CLEAR_SYMBOLS The currently loaded symbols will be cleared before the next program is loaded
SYMBOLS_ONLY Only the prerequisite program's symbols will be loaded.  No code/data will be loaded.
NO_RESET_BEFORE_LOAD The core will not be reset before the prerequisite program is loaded.  If this option is not specified, the core will be reset before the load.
RUN_AFTER_LOAD A temporary breakpoint will be set at the prerequisite program's ___lib_prog_term label and the program will be run to that breakpoint.

Preload Program

To specify a prerequisite program, a path that points to the DXE file relative to the CCES installation directory is necessary.
For example, Blackfin\Examples\drivers\flash\BF506F\bf506f_flash.dxe.

Simplification

If prerequisite options are not explicitly specified when using the core command, CCES Runner will see if default preloads are available and load them automatically.

Example:

When running an ADSP-SC589 Core 0 project:

--core "0,C:\workspace\ADSP-SC589_Core0\Debug\ADSP-SC589_Core0"

This command would also load the prerequisite program to set up clocks and DMC settings, so that the debugger is able to load the user’s application to external memory, as

--core "0,EMU|KIT|CLEAR_SYMBOLS|RUN_AFTER_LOAD|SHARC\ldr\ezkitSC589_preload_core0_v01,
        C:\workspace\ADSP-SC589_Core0\Debug
\ADSP-SC589_Core0"

Reading From and Writing Data To Files and Memory

The --datafile option can be used to initialize memory from data stored in a file on the host as well as save data from memory back to a host file. The argument to --datafile is a comma separated string with 8 options as follows:


--datafile "<core>,<direction>,<filename>,<format>,<symbol>,<length>,<stride>,<breakpoint_symbol>"

Options

Argument Description
core The zero based core id to read data from or write data to
direction

One of two values:

in - to specify that data should be loaded from a file and written to target memory after the application is loaded but before it is executed

out - to specify that data should be read from target memory and written to a file upon termination of the application

filename The path and filename of the file on the host to read from or write to
format

binary or binary:le - Specifies a binary file in little-endian format

binary:be - Specifies a binary file in big-endian format

<other> - Specifies a text file format from those listed via the --list-memformats option

symbol A global symbol name or hexadecimal address in your application for the specified core to which data will be read from or written to
length The number of values to read from or write to the file. Or it can be 'all' to specify that the entire file should be read when direction is 'in'.   
stride The stride value to use when reading from or writing to memory. A stride of 1 will use every value while 2 will use every other value and so on.
breakpoint_symbol (Optional) The symbol of a breakpoint to specify when this reading/writing operation happens.

 

Example 1 - Writing a File to Memory

This example reads 4096 values of data from a text file called input.dat which contains floating point formatted numbers on each line and writes it to core 0 memory starting at the address specified by stream_input before the application is run.


--datafile "0,in,input.dat,Floating Point 32 bit,stream_input,4096,1"
--datafile "0,in,input.dat,Floating Point 32 bit,0x001c0c4f,4096,1"

 

Example 2 - Writing Memory to a File

 

This example reads 1024 memory locations on core 0 starting at stream_output and writes it to a binary file called output.dat on the host. The file is written when the applications main() routine terminates.


--datafile "0,out,output.dat,binary,stream_output,1024,1"
--datafile "0,out,output.dat,binary,0x001c0c4f,1024,1"
 

Example 3 - Writing Memory to a File When a Specified Breakpoint is Hit

 

This example reads 1024 memory locations on core 1 starting at stream_output and writes it to a binary file called output.dat on the host. The file is written when the program runs and hits the specified breakpoint symbol 'BP'.


--datafile "1,out,output.dat,binary,stream_output,1024,1,BP"
--datafile "1,out,output.dat,binary,0x001c0c4f,1024,1,BP"

 

Listing Valid Memory Formats

 

Since different processor types have different file formats that they understand the list can vary from part to part. To see the list of valid --datafile <format> options you can use the --list-memformats option in conjunction with a chosen target, platform and processor. This option takes a single parameter called <core> which specifies the zero based core in the processor for which to list formats.

 

$ CCES_Runner.exe \
  --target "Sharc Emulators/EZ-KIT Lites" \
  --platform "ADSP-21489 via ICE-2000" \
  --processor "ADSP-21489" \
  --list-memformats 0

  32 Bit Hexadecimal
  Binary
  Floating Point 32 bit
  Floating Point 40 bit
  Hexadecimal
  Octal
  Signed Fractional
  Signed Integer
  Unsigned Fractional
  Unsigned Integer

 

Setting Breakpoints

The --breakpoint option can be used to set a breakpoint at the specified. One breakpoint option can be used per core but multiple breakpoints can be set in one breakpoint option.

Example:

To set a breakpoint at address 0x001c0c4f, main() and adi_intComponents() for a core 0 program:

--breakpoint "0,0x001c0c4f,main,adi_initComponents"

Profile-Guided Optimization (PGO)


The --pgo command can be used to collect PGO output data in a specified file. Simulator only.

Example:

--pgo "C:\CCESWorkspace\ADSP-BF533\Debug\ADSP-BF533.pgo"

Note:

To find more information about Profile-Guided Optimization and Code Coverage, visit the help contents in CCES:

CrossCoreRegistered Embedded Studio 2.7.0 > SHARCRegistered Development Tools Documentation > C/C++ Compiler Manual for SHARCRegistered Processors > Optimal Performance from C/C++ Source Code > Analyzing Your Application

 

Debug Session Preferences


The --preferences command can be used to set preferences for your CCES Runner debug session. The --preferences command takes a white space delineated list of preferences with optional values.

Example:

To increase the JTAG frequency to 46Mhz when loading and running program(s) using an ICE-2000, add the following command to your CCES Runner command line: --preferences "jtagfrequency=46"

Specify inputs to CCES Runner using an input text file

The -@ or --config option can be used to specify an input text file containing the CCES Runner options.

For example, add the following to a file called options.txt:

target=ADSP-BF5xx Blackfin Family Simulators  
platform=ADSP-BF5xx Single Processor Simulator
processor=ADSP-BF504 
core=0,C:\tmp\bf.dxe
breakpoint=0,main,f1,0xffa00112
datafile=0,out,address-final.dat,Hexadecimal,0xff800598,1,1
datafile=0,out,name-final.dat,Hexadecimal,ga,1,1
datafile=0,out,name-initial.dat,Hexadecimal,ga,1,1,main
datafile=0,out,name-middle.dat,Hexadecimal,ga,1,1,0xffa00112
verbose=2
And specify -@ options.txt on the CCES Runner command line:

$ CCES_Runner.exe -@ options.txt

Specify a custom board support file

The --customboard option can be used to specify a custom board support file. A custom board support file can be used to override the default register reset values with custom memory-mapped registers.

For example,  --customboard BF527-custom.xml

Releases

1.1.0.16

  • Enhancement: improved CCES Runner time-out handling.

1.1.0.15

  • Enhancement: removed the need to specify a core id when only running one program. Improved load prerequisites handling.

1.1.0.14

  • Enhancement: better handling of SHARC processors without an ARM core.

1.1.0.13

  • Bug fix: CCES runner randomly fails using a simulator starget.

1.1.0.12

  • It is now possible to specify a custom board support file using the  --customboard option.

1.1.0.11

  • CCES Runner can now load an entire data file by specifying all in the data file option. For example,  --datafile 0,in,test.dat,binary,buf,all,1.

1.1.0.10

  • Bug fix: --breakpoint fails if symbol does not exist in the executable.

1.1.0.9

  • It is now possible to add your CCES Runner options to an input file and use that file on the CCES Runner command line with the -@ switch.

1.1.0.8

  • Dumping to a data file does not append to the file which means that a new data file is created each time a breakpoint it hit, the data dumped, and execution continues.
  • Fix for issues found by Coverity.
  • Eclipse feature/plugins versions bumped to 1.1.0.0.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.