Article Boot without CCES Audit

Question:

Is it possible to program the flash in boot-mode on the BF706 EZLITE without using CCES?

===============================

Answer:

From CCES 2.8.0 onward, the need for a CCES license has been removed from the CLDP. Users can now use the CLDP without having  separate license for each machine it is used on. But a full CCES install is still needed in order to use the CLDP however.

CrossCore Serial Flash Programmer (CCSFP)

CrossCore Serial Flash Programmer (CCSFP) is a standalone application for programming, erasing and re-programming the on-board flash of mixed-signal processors, via the UART interface.Future releases of CrossCore Serial Flash Programmer will be distributed as part of the CrossCore Utilities product.

For more details refer the below linked CrossCore® Utilities product page:

https://www.analog.com/en/design-center/evaluation-hardware-and-software/software/crosscore-utilities.html#software-overview

Please refer the below linked FAQ:
FAQ: How do I program flash on my target board using CrossCore Embedded Studio?
https://ez.analog.com/docs/DOC-2111

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.