CrossCore Embedded Studio STDIO: FAQ

  • Created
Was this helpful?
  • "DO_CYCLE_COUNTS" macro in CCES

    Question: While using cycle count program in CCES, it does not print number of cycles. Why? Answer: When running cycle count program, ensure that "DO_CYCLE_COUNTS" macro is specified in the Project Options…
  • Build Configuration settings in CCES

    Question: Why does the project always open in Debug mode upon reopening, even when it was previously set to Release mode? Answer: CrossCore Embedded Studio (CCES) stores the active build configuration…
  • Cache settings on SHARC-FX

    Question: Where can the cache settings be modified for SHARC-FX? Answer: In SHARC+ projects, the cache size settings are configured in the Startup Code/LDF Add-in. You can select different sizes, or…
  • CCES Debug configuration settings

    Question: i. How to create a common project property settings for both Debug and Release at a same time? Answer: If we need the setting update to be added to both debug and Release configurations, first…
  • CCES_HOME Environment variable

    1. CCES_HOME Environment variable Question Is it necessary to add CCES_HOME (specific CCES installation directory) in system environmental variable? Answer CCES_HOME can be used to overwrite internal…
  • Change output directory path of DXE. Audit

    Question : How to store the output “dxe” in the desired location when building the project? Answer: Set the output path for a DXE via the 'Output prefix' field in the Artifact tab. Follow the below…
  • Compare EV-SOMCRR-EZKIT and EV-SOMCRR-EZLITE

    1. Difference Between EV-SOMCRR-EZKIT and EV-SOMCRR-EZLITE Below is the comparison table which gives the better understanding about the difference between EV-SOMCRR-EZKIT and EV-SOMCRR-EZLITE. …
  • Create ASM project in CCES

    Question: How to create ASM project in CCES? Answer: Direct creation of ASM projects is not possible, as CCES only support creating C/C++ projects. So, create a new project for C/C++ and delete…
  • CrossCore Embedded Studio STDIO is slow, and interrupts processing of real world data Audit

    Question: When I use STDIO functions, such as printf, the process is slow and incoming data is missed. Why? --------------------------------------------- Answer: The slow stdio operations which…
  • Default qualifier for the output sections

    Question: What is the default section qualifier for output sections that are not specified, such as NO_INIT and ZERO_INIT? Answer: The assembler uses the default SHT_PROGBITS when section type identifier…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.