Question:
Explain the reason for error "Error: processor 'ADSP-21593' is not supported" when flash binary file using CLDP 2.10.1
Answer: The error will be resolved by removing CCES_HOME environment…
Question: How do I view a specific symbol in the CCES plot window?
Answer: 1. Connect the debug session and go to window->Show view->Plot window. In the Edit Data Set window, 2. Click on the 3 dots …
Question:
How can I add or remove tool switches via command-line build support?
Answer: We can use "-append-switch, -remove-switch and -replace-switch" options to add, remove and change tool switches…
Question:
Is there a way to force the compiler to allocate all memory to L1 by default rather than individually allocating each variable via #pragma section?
Answer:
If there is possibilty for program…
Question:
I used to use id=heap_lookup_name("seg_xxx") with heap_calloc to manage the custom heap space in my program in VDSP++.
But in CCES , the heap_lookup_name has been eliminated ,I'm wondering…
Question:
Do we have any standard function in CCES for create a delay in application?
Answer: This example performs a simple delay using an ASM function. The user-defined variable 'del_cycle' determines…
Question: How to view a *.map file generated for the ARM core?
Answer: There are tools available which allows to quickly inspect the MAP file generated by GNU toolchain. CCES uses GNU toolchain for ARM…
Question:
Is there any Cycle-Counting Macros available for ARM core similar to SHARC/Blackfin?
Answer:
Yes, Cycle-counting macros, similar to those available for SHARC and Blackfin, have been added…
Question:
While allocating a buffer in SDRAM of '1,20,96,000' in size @32bit with a data file memory allocation failure error ea1144 is observed. How to resolve error ea1144?
Ex : .var arr[12096000…
Question:
Is it possible to program the flash in boot-mode on the BF706 EZLITE without using CCES?
===============================
Answer:
From CCES 2.8.0 onward, the need for a CCES license has…