ADSP-SC59x: FAQs

  • Created
  • Updated
Was this helpful?
  • Flash Read/Write using SPI APIs

    Question: Flash Read/Write in SPI DMA mode for SC594 Answer: This example demonstrates how to communicate with the flash chip using SPI in DMA mode, supporting both single and dual modes. It has been…
  • FreeRTOS Task Execution Tracing

    Question: How to use Application Task Tag feature in FreeRTOS Answer: The Application Task Tag feature in FreeRTOS allows attaching a custom function (trace hook) to each task, which is automatically…
  • FreeRTOS Task Stack Memory Mapping on ADSP-21593

    Question: FreeRTOS Task Stack Memory Mapping on ADSP-21593 Answer: This FAQ explains the Task Stack Memory Mapping on ADSP-21593 processor. FreeRTOS supports two methods of task creation: …
  • RTOS Task Stack Memory Mapping

    This FAQ explains the Task Stack Memory Mapping and Stack overflow detection in ADSP-SC594 A5 core FreeRTOS. Introduction: FreeRTOS supports two methods of task creation: Dynamic Task Creation…
  • How can I create custom multi-processor platforms for ADSP-SC598 family of parts? Audit

    If there is an ADSP-SC598 family processor as part of a custom scan chain, contact processor.tools.support@analog.com for assistance in debugging this setup.
  • How can I debug my ADSP-SC598 family part heterogeneously (simultaneous debug of the Cortex-A55 and SHARC cores)?

    CrossCore Embedded Studio 2.11.0 and newer support heterogeneous debugging for the ADSP-SC598 family of parts via CrossCore Launch Group debug configurations. The ARM Cortex A55 core is debugged via GDB…
  • SC-594: Buffer Address Sharing via RPMsg Lite

    Question: How to get destination core's buffer address using RPMsg Protocol Answer: The attached multicore audio talk-through example demonstrates how to configure and use the RPMsg Lite protocol…
  • Software Timer in FreeRTOS

    Question: Demonstration of Using a Software Timer API in FreeRTOS on the SC594 Platform Answer: This example demonstrates how to configure software timers in FreeRTOS. Three software timers are created…
  • SPDIF Digital Output

    Question: Example Project demonstrates SPDIF Digital Output from Analog Audio Input Answer: The attached example project demonstrates how to convert analog audio input to a digital SPDIF output.…
  • SPI core mode APIs

    Question: How to use SPI core mode APIs? Answer: The attached example shows how to use SPI core mode APIs between two Sharc cores in SC598 Eval board and between two Eval boards . Example1: (ADSP…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.