Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the AI Power Storm: Part 2 of 3

    Let’s peel back the curtain on how Analog Devices (ADI) is leading the charge, crafting power solutions that not only keep up with AI’s appetite but redefine...

     

    TIA Me Up, But Keep It Stable: Part 2 of 3

    Imagine trying to measure a current so tiny that it’s almost invisible. How is that even possible? How do we even convert that current signal into something...

    Latest Blogs

    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
    • ​​Where Errors Lurk in the GMSL Signal Chain​
    • Achieving Power Over Data with RS-485 Transceivers
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
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents What types of capacitors are good to use in the analog audio signal path?
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • -SigmaDSP: FAQ
    • Booting a SigmaDSP from a microcontroller with no C compiler
    • Calculating Filter Coefficients to Store in a Microcontroller
    • Can I program multiple SigmaDSPs in parallel using one USBi?
    • Can I use SigmaDSP to decode MP3/WAV/AAC?
    • Can I write C or assembly code for SigmaDSP in SigmaStudio?
    • Can SigmaDSP do frequency-domain processing like FFT or pitch shift?
    • Can we bundle SigmaStudio with our product design?
    • Creating a delay after startup
    • Developing custom algorithms and/or using 3rd party algorithms
    • How can I estimate MIPS/Memory resource on SigmaDSP?
    • How do I create the microcontroller code to interface to my SigmaDSP?
    • How do I start a timer after power-on, or when the input signal goes away?
    • How many instructions can be executed per sample in SigmaDSP?
    • Memory requirements for booting a SigmaDSP with a microcontroller
    • Monitoring average and instantaneous signal levels
    • Playing audio samples in SigmaDSP
    • SigmaDSP PCB Layout Best Practices
    • SigmaDSP Products and Evaluation Boards - ROHS and REACH Compliance
    • SigmaStudio 3.4 Released
    • Updating SigmaDSP Parameter with a Microcontroller
    • Using two SigmaDSP evaluation boards simultaneously with one USBi board
    • Welcome to the SIGMADSP Processors and SIGMASTUDIO Development tool community
    • What are the number formats for SigmaDSP?
    • What is the step size for audio delay in a SigmaDSP?
    • What types of capacitors are good to use in the analog audio signal path?
    • Where can I buy a SigmaDSP Evaluation Board or USBi (EVAL-ADUSB2EBZ)?
    • Which SigmaDSP ICs support selfbooting from an EEPROM?
    • Which SPI Mode is used by SigmaDSP Devices?
    • Why isn't a software/documentation CD included with my evaluation board?
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

What types of capacitors are good to use in the analog audio signal path?

In general, there are 3 types of capacitors that will be available in the values that are appropriate as AC coupling in most signal paths: electrolytic, tantalum and ceramic. Each has strengths and weaknesses.

Electrolytic capacitors are generally the best performing for this purpose. They are very linear when biased by the Common Mode voltages present in most SigmaDSP audio paths and their low ESR (Equivalent Series Resistance) makes them attractive as an 'invisible' component when designing a circuit. They are fairly low cost as well. However, electrolytic capacitors have quite a large footprint and they will suffer from degradation of value and performance over time - especially in a high temperature environment. They literally 'dry out' and become a high pass filter in the signal path. High temperature versions are available and will hold up well over a long period of time.

Tantalum capacitors are a reasonable alternative, however they are more expensive than electrolytics and are not available in as many values. As polarized capacitors, they must also be biased, however I have not found them to be as linear in an audio path as electrolytic capacitors. Some people say they "don't sound as good," however static single-tone distortion tests might not reveal any differences. On the positive side, tantalums do not dry out and so are appropriate for a long term high temperature environment. They are generally smaller than electrolytics for the same value.

Both of the non-ceramic types will hold their capacitive value under use condition, unlike ceramics....

Ceramic capacitors are generally not recommended for use as AC coupling in audio. They are attractive because of the size, cost and low ESR. However, when most ceramic capacitors are biased, the capacitive rating can decrease by as much as 50%! The higher grade (X7R) types suffer less from this, but you should be aware that a 1 uF might be acting like a 0.68uF in the circuit. We have also found that ceramic capacitors suffer from microphonic effects: the audio passing through the part will actually physically resonate and cause distortion! I would only use ceramic capacitors in the audio path where performance is not an issue, but size and cost are your higher priority. NP0 and C0G are the best of the ceramics, however I don't think you will find these types available in appropriate values.

You will also see some references to film capacitors for use as AC coupling in audio. While they are stellar performers, they are very large in size for the rated value. I have also had a great deal of trouble with the SMD versions of these parts surviving assembly and reflow using standard automated assembly techniques.

The value of your capacitor will be determined by the impedance of the circuit and the desired low-frequency response. To choose a voltage ratings, you need to consider the bias voltage plus the AC voltage swing of the audio signal. I would be conservative and double this total value - higher values sometimes come in the same size package, have a lower ESR (a good thing) and will be less likely to fail in case other components in the circuit fail.

This FAQ was generated from the following discussion: Choosing capacitors  for audio path

Tags: capacitors coupling ceramic schematic electrolytic layout dielectric caps SigmaDSP tantalum esr audio analog Show More
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: Choosing capacitors  for audio path
    ColemanR
    Hi Farhad, Thank you for your inquiry about capacitors in the audio path around our SigmaDSP parts. In general, there are 3 types of capacitors that will be available in the values that are appropriate...
  • RE: Question about ADAU1966A
    DaveThib
    Hello lefeng, This is a huge topic for discussion and there have been many articles written about this subject. This depends on the actual use of the capacitor. In general, we used a lot of aluminum...
  • RE: Question about ADAU1966A
    DaveThib
    Hello lefeng, Again, these are difficult questions for me to answer. I am not an expert on capacitors but I do have some experience in choosing capacitors for audio performance. Keep in mind that my...
 
Related Content
  • RE: Choosing capacitors  for audio path
    ColemanR
    Hi Farhad, Thank you for your inquiry about capacitors in the audio path around our SigmaDSP parts. In general, there are 3 types of capacitors that will be available in the values that are appropriate...
  • RE: Question about ADAU1966A
    DaveThib
    Hello lefeng, This is a huge topic for discussion and there have been many articles written about this subject. This depends on the actual use of the capacitor. In general, we used a lot of aluminum...
  • RE: Question about ADAU1966A
    DaveThib
    Hello lefeng, Again, these are difficult questions for me to answer. I am not an expert on capacitors but I do have some experience in choosing capacitors for audio performance. Keep in mind that my...