Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents How can I change parameters on-the-fly in an application without SigmaStudio?
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • -SigmaStudio: FAQ
    • Can I have multiple versions of SigmaStudio installed simultaneously?
    • How are the audio inputs routed in SigmaStudio's Input cell?
    • How can I change parameters on-the-fly in an application without SigmaStudio?
    • How do I change the sample rate of my SigmaStudio system?
    • How do I report a SigmaStudio bug?
    • New SigmaStudio 3.3 Beta Version Available
    • New SigmaStudio Download Site
    • Sigma 300 (ADAU145x) Exponential Slewing
    • SigmaStudio consulting services...
    • The ADAU1372 is not on the list of compatible processors or under Processors/DSPs on Sigmastudio 3.11.1 or 3.11. Can you please tell me how I can use the EVAL board with ADAU1372?
    • Third Party Algorithm Plugins in SigmaStudio
    • True peak-to-peak detection in SigmaStudio
    • Using compressors to avoid output clipping
    • Using stopwatch with feedback loop to create periodic test signal
    • What operating systems are supported to run SigmaStudio?
    • Where can I download SigmaStudio?
    • Where can I find a description of the changes made in the latest version of SigmaStudio?
    • Where can I send my questions I don't want to post in a public forum?
    • Why can't I control any of the knobs or sliders in my SigmaStudio project?
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

How can I change parameters on-the-fly in an application without SigmaStudio?

There are several options for calculating the parameter values you should download to the SigmaDSP control port. Here are a few examples:

  • Open the capture window in SigmaStudio and change a parameter to a new value. The capture window shows you what address to download to and what values to write. It will also show if the write should be a block write, individual write, or safeload write.
  • Use the filter coefficient calculator (Tools...Fixed Point Filter Table Generator) to calculate values for filter coefficients. You can export these and include them in your microcontroller compilation.
  • Use the coefficient calculation equations in the SigmaStudio help file to calculate your own coefficients. You can also implement these equations in a system's microcontroller to calculate coefficients during system operation.
  • Use programs like MatLab to calculate IIR coefficients.

For complete listings of parameter addresses and values in a number of formats, use the "Export System Files" function in SigmaStudio after compiling your project. The "Export System Files" button is located in the main toolbar.

This FAQ was generated from the following discussion: How can I change parameters on-the-fly in an application without SigmaStudio?

Tags: adau1702 adau1401 ad1941 i2c adau1446 spi microcontroller adau1442 adau1445 parameters communication adau1761 adau1701 Show More
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: How can I change parameters on-the-fly in an application without SigmaStudio?
    ADIApproved
    There are several options for calculating the parameter values you should download to the SigmaDSP control port. Here are a few examples: Open the capture window in SigmaStudio and change a parameter...
  • How can I change parameters on-the-fly in an application without SigmaStudio?
    ADIApproved
    My target system will have a microcontroller which i will use to control the signal processing parameters in real-time. How do I calculate the values of the parameters I want to update?
  • Calculating Filter Coefficients to Store in a Microcontroller
    Sara Collins
    Recently there have been some email support requests regarding the calculation of filter coefficients (and other types of parameters) for storage in a microcontroller. The basic idea is to store a table...
 
Related Content
  • RE: How can I change parameters on-the-fly in an application without SigmaStudio?
    ADIApproved
    There are several options for calculating the parameter values you should download to the SigmaDSP control port. Here are a few examples: Open the capture window in SigmaStudio and change a parameter...
  • How can I change parameters on-the-fly in an application without SigmaStudio?
    ADIApproved
    My target system will have a microcontroller which i will use to control the signal processing parameters in real-time. How do I calculate the values of the parameters I want to update?
  • Calculating Filter Coefficients to Store in a Microcontroller
    Sara Collins
    Recently there have been some email support requests regarding the calculation of filter coefficients (and other types of parameters) for storage in a microcontroller. The basic idea is to store a table...