Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents How do I create the microcontroller code to interface to my SigmaDSP?
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • -SigmaDSP: FAQ
    • Booting a SigmaDSP from a microcontroller with no C compiler
    • Calculating Filter Coefficients to Store in a Microcontroller
    • Can I program multiple SigmaDSPs in parallel using one USBi?
    • Can I use SigmaDSP to decode MP3/WAV/AAC?
    • Can I write C or assembly code for SigmaDSP in SigmaStudio?
    • Can SigmaDSP do frequency-domain processing like FFT or pitch shift?
    • Can we bundle SigmaStudio with our product design?
    • Creating a delay after startup
    • Developing custom algorithms and/or using 3rd party algorithms
    • How can I estimate MIPS/Memory resource on SigmaDSP?
    • How do I create the microcontroller code to interface to my SigmaDSP?
    • How do I start a timer after power-on, or when the input signal goes away?
    • How many instructions can be executed per sample in SigmaDSP?
    • Memory requirements for booting a SigmaDSP with a microcontroller
    • Monitoring average and instantaneous signal levels
    • Playing audio samples in SigmaDSP
    • SigmaDSP PCB Layout Best Practices
    • SigmaDSP Products and Evaluation Boards - ROHS and REACH Compliance
    • SigmaStudio 3.4 Released
    • Updating SigmaDSP Parameter with a Microcontroller
    • Using two SigmaDSP evaluation boards simultaneously with one USBi board
    • Welcome to the SIGMADSP Processors and SIGMASTUDIO Development tool community
    • What are the number formats for SigmaDSP?
    • What is the step size for audio delay in a SigmaDSP?
    • What types of capacitors are good to use in the analog audio signal path?
    • Where can I buy a SigmaDSP Evaluation Board or USBi (EVAL-ADUSB2EBZ)?
    • Which SigmaDSP ICs support selfbooting from an EEPROM?
    • Which SPI Mode is used by SigmaDSP Devices?
    • Why isn't a software/documentation CD included with my evaluation board?
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

How do I create the microcontroller code to interface to my SigmaDSP?

Each microcontroller is different, so the answer to this question will vary greatly depending on what architecture you have chosen. However, SigmaStudio includes some functionality that allows you to generate C-compatible header files that should greatly reduce the complexity of microcontroller integration and development.

Attached to this message is a brief tutorial in the form of a PDF-converted PowerPoint  presentation. There is also a zip file containing the full design and code files for an ADAU1761  in a system with an ARM Cortex M3 microcontroller. By reading the presentation and examining the files, you should be able  to see how the framework macros are created and how the sequencer is used  to define operating modes and create download sequences for the microcontroller.  At this stage, it's not fully documented, but it should be good enough to get you started with a working example.

The PDF and project files are attached. Please take a look.

Also, an example hardware design with an ARM Cortex M3 microcontroller and two ADAU1761 SigmaDSPs is included in the attached PDF file.

Attachments:
ADAU1761_Demo.zip
SigmaStudioBasicuCIntegrationTutorial.pdf
ARM_ADAU1761_DesignFiles.zip
Tags: c header microcontroller sequencer sigmastudio SigmaDSP Show More
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: So how about all this programming the host microcontroller stuff, anyhow?
    ADIApproved
    Hi everyone, Sorry, this is long overdue. I currently have a brief tutorial in the form of a PDF-converted PowerPoint presentation. I also have the full design and code files for an ADAU1761 in a system...
  • RE: sigmaDsp cofig by microcontroller use I2C?
    ADIApproved
    We have a tutorial using an ARM Cortex processor available here: How do I create the microcontroller code to interface to my SigmaDSP? The example contains a tutorial and full source code. If you...
  • RE: Configuring the Sampling Rate of the ADAU1761
    JohnTo
    Hello Jacob, The following FAQ shows an ADAU1761 download example from a Cortex-M3 based microcontroller (STM32 processor using the Keil ARM tools). This is just plain C code with no operating system...
 
Related Content
  • RE: So how about all this programming the host microcontroller stuff, anyhow?
    ADIApproved
    Hi everyone, Sorry, this is long overdue. I currently have a brief tutorial in the form of a PDF-converted PowerPoint presentation. I also have the full design and code files for an ADAU1761 in a system...
  • RE: sigmaDsp cofig by microcontroller use I2C?
    ADIApproved
    We have a tutorial using an ARM Cortex processor available here: How do I create the microcontroller code to interface to my SigmaDSP? The example contains a tutorial and full source code. If you...
  • RE: Configuring the Sampling Rate of the ADAU1761
    JohnTo
    Hello Jacob, The following FAQ shows an ADAU1761 download example from a Cortex-M3 based microcontroller (STM32 processor using the Keil ARM tools). This is just plain C code with no operating system...