Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents How do I execute a software safeload write?
  • Q&A
  • Docs/FAQs
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • -How do I execute a software safeload write?: FAQ
    • How do I execute a software safeload write?
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

How do I execute a software safeload write?

In order to use software safeload to write data to parameter RAM, at least three writes must be performed. First, the data is loaded into the safeload data registers (addresses 0x0001 through 0x0005), then the safeload target address register (address 0x0006), and finally the number of words / trigger register (address 0x0007). So, in order to execute a safeload write, there are at least 3 register writes that need to occur.

Single address safeload write

For example, if I wanted to write one word of data to address 0x000B…

There are 3 total writes:

  • Address 0x0001, write 4 bytes of data.
  • Address 0x0006, write 0x0000000A (this is my target address of 0x000B minus one).
  • Address 0x0007, write 0x00000001 (because you are writing one word of data).

This will trigger the safeload write on the next frame.

Note that the target address is actually shifted down by one, as mentioned in the datasheets for devices using software safeload. So, even though I’m writing to address 0x000B, I write 0x000A to the target address register.

Multiple address safeload write

Here’s another example, where I will write 3 words of data instead of 1 word. The target addresses for the 3 words of data are 0x001C, 0x001D, and 0x001E.

There are 5 total writes:

  • Address 0x0001, write 4 bytes of data that will be safeloaded to address 0x001C.
  • Address 0x0002, write 4 bytes of data that will be safeloaded to address 0x001D.
  • Address 0x0003, write 4 bytes of data that will be safeloaded to address 0x001E.
  • Address 0x0006, write 0x0000001B (this is 0x001C minus one).
  • Address 0x0007, write 0x00000003 (because you are writing three words of data).

This will trigger the safeload write on the next frame.

Note that multi-word safeload writes can only be accomplished when the target addresses are sequential.

This FAQ was generated from the following discussion: Software safeload examples

Tags: i2c adau1446 spi adau1442 adau1445 adau1761 write ram safeload Show More
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • Software safeload examples
    ADIApproved
    In order to use software safeload to write data to parameter RAM, at least three writes must be performed. First, the data is loaded into the safeload data registers (addresses 0x0001 through 0x0005),...
  • RE: ADAU1761 safeload
    ADIApproved
    You should write an integer value to parameter RAM address 0x0007 to trigger the safeload. This means that to safeload one word, you should write 0x00 0x00 0x00 0x01 to address 0x0007, or in your example...
  • Question about Software Safeload Write Feature for Sigma DSP
    Tingting1992
    Hi, I am checking this page. How do I execute a software safeload write? - Documents - SigmaDSP Processors & SigmaStudio Dev. Tool - EngineerZone (analog.com) ============ In order to use software...
 
Related Content
  • Software safeload examples
    ADIApproved
    In order to use software safeload to write data to parameter RAM, at least three writes must be performed. First, the data is loaded into the safeload data registers (addresses 0x0001 through 0x0005),...
  • RE: ADAU1761 safeload
    ADIApproved
    You should write an integer value to parameter RAM address 0x0007 to trigger the safeload. This means that to safeload one word, you should write 0x00 0x00 0x00 0x01 to address 0x0007, or in your example...
  • Question about Software Safeload Write Feature for Sigma DSP
    Tingting1992
    Hi, I am checking this page. How do I execute a software safeload write? - Documents - SigmaDSP Processors & SigmaStudio Dev. Tool - EngineerZone (analog.com) ============ In order to use software...