Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the AI Power Storm: Part 2 of 3

    Let’s peel back the curtain on how Analog Devices (ADI) is leading the charge, crafting power solutions that not only keep up with AI’s appetite but redefine...

     

    TIA Me Up, But Keep It Stable: Part 2 of 3

    Imagine trying to measure a current so tiny that it’s almost invisible. How is that even possible? How do we even convert that current signal into something...

    Latest Blogs

    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
    • ​​Where Errors Lurk in the GMSL Signal Chain​
    • Achieving Power Over Data with RS-485 Transceivers
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
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents SigmaDSP PCB Layout Best Practices
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • -SigmaDSP: FAQ
    • Booting a SigmaDSP from a microcontroller with no C compiler
    • Calculating Filter Coefficients to Store in a Microcontroller
    • Can I program multiple SigmaDSPs in parallel using one USBi?
    • Can I use SigmaDSP to decode MP3/WAV/AAC?
    • Can I write C or assembly code for SigmaDSP in SigmaStudio?
    • Can SigmaDSP do frequency-domain processing like FFT or pitch shift?
    • Can we bundle SigmaStudio with our product design?
    • Creating a delay after startup
    • Developing custom algorithms and/or using 3rd party algorithms
    • How can I estimate MIPS/Memory resource on SigmaDSP?
    • How do I create the microcontroller code to interface to my SigmaDSP?
    • How do I start a timer after power-on, or when the input signal goes away?
    • How many instructions can be executed per sample in SigmaDSP?
    • Memory requirements for booting a SigmaDSP with a microcontroller
    • Monitoring average and instantaneous signal levels
    • Playing audio samples in SigmaDSP
    • SigmaDSP PCB Layout Best Practices
    • SigmaDSP Products and Evaluation Boards - ROHS and REACH Compliance
    • SigmaStudio 3.4 Released
    • Updating SigmaDSP Parameter with a Microcontroller
    • Using two SigmaDSP evaluation boards simultaneously with one USBi board
    • Welcome to the SIGMADSP Processors and SIGMASTUDIO Development tool community
    • What are the number formats for SigmaDSP?
    • What is the step size for audio delay in a SigmaDSP?
    • What types of capacitors are good to use in the analog audio signal path?
    • Where can I buy a SigmaDSP Evaluation Board or USBi (EVAL-ADUSB2EBZ)?
    • Which SigmaDSP ICs support selfbooting from an EEPROM?
    • Which SPI Mode is used by SigmaDSP Devices?
    • Why isn't a software/documentation CD included with my evaluation board?
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

SigmaDSP PCB Layout Best Practices

Good layout practices are of key importance when designing SigmaDSP system PCBs.

  • First of all, a solid ground plane is a necessity in order to  maintain signal integrity and minimize EMI radiation. If you have two  ground planes, I would recommend using stitching vias spead evenly  throughout the board in order to connect them.
  • Power supply high frequency decoupling capacitors should be placed  as close as possible to the respective power and ground pins, on the  same side of the board as the SigmaDSP IC. There should be no vias  between the pins and the decoupling caps. Please see the following excerpts from the ADAU144x datasheet for more detail.

  • Typically, we use a single 100 nF capacitor for each power-ground  pin pair. However, if there is excessive high frequency noise in the  system, an additional 10 nF capacitor can be used in parallel. In that  case, the 10 nF capacitor should be closest, and the thermal connections  should be on the far side of the 100 nF capacitor.

  • 10 uF capacitors should be used for each named supply (DVDD, AVDD,  IOVDD, etc) in order to provide a current reservoir in case of sudden  current spikes.

  • If ferrite beads are desired for supply isolation, the beads should always be placed outside of the local high frequency decoupling capacitors, like in the following diagram. If the ferrite beads are instead placed between the supply pin and the decoupling capcitor, high frequency noise will be reflected back into the IC since it does not have a suitable return path to ground, and this will increase EMI and create noisy supplies.

  • The proximity of components to the IC is important. Here is my  suggested order of priority which should be followed when placing components. The  top of the list begins with the components that should be placed closest to the IC (those in bold have highest priority), and the bottom of the list has the components that can (if absolutely necessary) be placed further away.
    • 10 nF high frequency decoupling capacitors
    • 100 nF high frequency decoupling capacitors
    • PLL filter components
    • Crystal
    • Current reservoir capacitors
  • ICs with exposed thermal paddles require extra attention during PCB design. A copper square matching the geometry of the exposed pad should be placed on all layers the PCB, with thermal vias connecting the layers in order to maximize heat transfer.

This FAQ was generated from the following discussion: in case of crash

Tags: noise pcb layout SigmaDSP bypass
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: in case of crash
    ADIApproved
    Good layout practices are of key importance when dealing with a noisy system. First of all, a solid ground plane is a necessity in order to maintain signal integrity and minimize EMI radiation. I have...
  • Power supplies, capacitors, and application schematics
    Sara Collins
    In SigmaDSP datasheets, the pin description table often has a statement like the following: This pin should be decoupled to DGND with a 100nF capacitor. However, if you look at the application circuit...
  • RE: Power supplies, capacitors, and application schematics
    ADIApproved
    There are two (or more) capacitors connected to each supply. One (or more) is a "High Frequency Decoupling" capacitor (100 nF = 0.1 uF), and the other is a "Current Reservoir" capacitor (10 uF). The...
 
Related Content
  • RE: in case of crash
    ADIApproved
    Good layout practices are of key importance when dealing with a noisy system. First of all, a solid ground plane is a necessity in order to maintain signal integrity and minimize EMI radiation. I have...
  • Power supplies, capacitors, and application schematics
    Sara Collins
    In SigmaDSP datasheets, the pin description table often has a statement like the following: This pin should be decoupled to DGND with a 100nF capacitor. However, if you look at the application circuit...
  • RE: Power supplies, capacitors, and application schematics
    ADIApproved
    There are two (or more) capacitors connected to each supply. One (or more) is a "High Frequency Decoupling" capacitor (100 nF = 0.1 uF), and the other is a "Current Reservoir" capacitor (10 uF). The...