Power Management Fundamentals II Session 4: Isolated Converters Explained

    What does isolation mean for power topologies? Let's review what galvanic isolation means and go through the terminology and standards. We'll explore isolation...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ296 about repairing an equation in a digital display

      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

     

    The 5 Advantages of Hardware Fault Tolerance

    In IEC 61508, HFT stands for “ H ardware F ault T olerance”. HFT of one or higher means that there is no single fault that will cause a safety function...

    Latest Blogs

    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
    • ​​Channel Specification: The Key to GMSL Compliance​
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
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents ADAU1701: ADC resistor values for higher sample rates
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • -ADAU1701: FAQ
    • ADAU1701 Input and Output Signal Routing
    • ADAU1701: ADC resistor values for higher sample rates
    • Implementing Safeload Writes on the ADAU1701
    • My 2IN4OUT Proto with SPDIF based on ADAU1701
    • Setting the PLL mode for the ADAU1701 at different sample rates
    • Thoughts on using index selectable filters...
    • Using hardware data capture (trap) registers with the DSP Readback cell (AD1940, ADAU1701)
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • +SigmaDSP: FAQ
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

ADAU1701: ADC resistor values for higher sample rates

As explained in the datasheet, the series resistors on the ADC inputs only need to be changed "is if a sampling rate other than 48 kHz is used." That being said, the definition of "sample rate" used here is somewhat ambiguous.

In some types of DSP (or codecs), in order to increase or decrease the sample rate, you simply scale the clock signals accordingly. For example, if you're feeding a 12.288 MHz master clock into the system for a 48 kHz sample rate, then you can simply scale that down by 8.125% to 11.2896 MHz for a 44.1 kHz sample rate, or double it to 24.576 MHz for a 96 kHz sample rate, etc... In many kinds of ICs, you are free to do this (as long as you stay within the boundaries of allowable clock frequencies) and all of the internally generated clocks will simply scale accordingly.

The ADAU1701 is a bit different. The PLL takes in a master clock and divides it down before multiplying it up to a much higher frequency. For a 48 kHz sample rate, the DSP core clock is 1024 * 48000 = 49.152 MHz. Now, when you want to use a 96 kHz sample rate, logically you might assume that the core clock doubles to 98.304 MHz. However, this is not the case for the ADAU1701. Its DSP core clock can only run up to somewhere in the 50 MHz range before things start to break down and function incorrectly. Scaling down for a 44.1 kHz sample rate is not a problem (the DSP core clock can easily run at 44.1584 MHz.

So, an alternate method is used for higher sample rates. For 96 kHz (which we refer to as "double rate" or "dual rate" in some other SigmaDSP datasheets), the DSP core simply grabs a sample twice as often as it did at 48 kHz. This also makes the interpolation and decimation filters for the converters run twice as fast, and has the side effect that the DSP core can only execute half as many instructions per sample as it could at the "normal rate" of 48 kHz.

Quad rate is possible as well, using the same method. The DSP core quadruples the rate at which it grabs samples from the converters and serial ports, and the interpolation and decimation filters do the same. Instead of scaling the frequency up or down of all of the clocks in the system, you're simply doubling or quadrupling the clock frequencies for certain subsystems.

That being said, the explanation regarding the ADC resistors refers more to the case I originally described above, where you might be running your system at 44.1 kHz or maybe at some strange non-standard rate like 49 kHz or 42 kHz. In that case, you're literally scaling the frequency of the MCLK, so the ADC resistor values need to scale as well.

Conversely, if you are running at 96 kHz, the MCLK frequency itself remains unchanged, and you're simply doubling the rate of the DSP core and converter filters. In that case, you only need to change a register setting, and no hardware changes are required.

The ADC is oversampling, clocked at a constant factor of the core clock regardless of single, dual, or quad rate modes, and the decimation is just occurring with 1/2 or 1/4 as many samples to compensate. It is the actual sampling rate of the converters which matters, and that is not affected by dual or quad rate modes.

In summary, the ADC_RES values for 48 kHz, 96 kHz and 192 kHz should be the same, because the core clock frequencies are the same in both cases.

[Edited 2012.03.01 to include nickw's corrections and comments]

This FAQ was generated from the following discussion: ADAU1701: ADC resistor values for higher sample rates

Tags: adc noise adau1701 sample_rate resistor
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: ADAU1701: ADC resistor values for higher sample rates
    ADIApproved
    Hi Steve, and welcome to the forum. Fortunately, I think I know the exact reason why this is happening! Unfortunately, I think it points out a lack of clarity in our datasheet. As explained in the...
  • RE: ADAU1701 Clocking and PLL
    ADIApproved
    This thread might help to clear up some confusion. Just to be clear, the core is always running at 49.152 MHz, but in the case of dual-rate or quad-rate processing, you're simply ordering the DSP to...
  • How do I change the sample rate of my SigmaStudio system?
    stephenv
    In order to change the sample rate of a system, follow these steps: Setting Software Sample Rate Locate the sample rate section of the toolbar. Click the drop-down box, and select a new sample...
 
Related Content
  • RE: ADAU1701: ADC resistor values for higher sample rates
    ADIApproved
    Hi Steve, and welcome to the forum. Fortunately, I think I know the exact reason why this is happening! Unfortunately, I think it points out a lack of clarity in our datasheet. As explained in the...
  • RE: ADAU1701 Clocking and PLL
    ADIApproved
    This thread might help to clear up some confusion. Just to be clear, the core is always running at 49.152 MHz, but in the case of dual-rate or quad-rate processing, you're simply ordering the DSP to...
  • How do I change the sample rate of my SigmaStudio system?
    stephenv
    In order to change the sample rate of a system, follow these steps: Setting Software Sample Rate Locate the sample rate section of the toolbar. Click the drop-down box, and select a new sample...