Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
SigmaDSP Processors & SigmaStudio Dev. Tool
  • Processors & DSP
SigmaDSP Processors & SigmaStudio Dev. Tool
Documents Can I use SigmaDSP to decode MP3/WAV/AAC?
  • Q&A
  • File Uploads
  • Members
  • Tags
  • Cancel
  • Documents
  • SigmaDSP YouTube Channel - Dave Thib
  • +AD193x: FAQ
  • +ADAU1401AEBZ: FAQ
  • +ADAU144x: FAQ
  • +ADAU1452: FAQ
  • +ADAU145x: FAQ
  • +ADAU1701: FAQ
  • +ADAU1701MINIZ- FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADI: FAQ
  • +AN-951: FAQ
  • +bitwise logic: FAQ
  • +Compressor Table Format: FAQ
  • +Creating a simple balance crossfade control: FAQ
  • +Creating constant-dB envelope decay using an existing linear decay algorithm: FAQ
  • +Crossover with more than 3 bands: FAQ
  • +E2PROM: FAQ
  • +EEPROM: FAQ
  • +EVAL DAU144XEBZ: FAQ
  • +EVAL-ADAU1781Z: FAQ
  • +Excluding Cells from the Exported System Files: FAQ
  • +GPIO button: FAQ
  • +GPIOs or Aux ADCs: FAQ
  • +How do I execute a software safeload write?: FAQ
  • +IIR coefficient filter: FAQ
  • +IIR filter: FAQ
  • +Peak Full Range Compressor: FAQ
  • +Preserving "Ear-candy": FAQ
  • +Push Button Volume: FAQ
  • +self-boot EEPROM image: FAQ
  • +Sigma300 Family Products: FAQ
  • -SigmaDSP: FAQ
    • Booting a SigmaDSP from a microcontroller with no C compiler
    • Calculating Filter Coefficients to Store in a Microcontroller
    • Can I program multiple SigmaDSPs in parallel using one USBi?
    • Can I use SigmaDSP to decode MP3/WAV/AAC?
    • Can I write C or assembly code for SigmaDSP in SigmaStudio?
    • Can SigmaDSP do frequency-domain processing like FFT or pitch shift?
    • Can we bundle SigmaStudio with our product design?
    • Creating a delay after startup
    • Developing custom algorithms and/or using 3rd party algorithms
    • How can I estimate MIPS/Memory resource on SigmaDSP?
    • How do I create the microcontroller code to interface to my SigmaDSP?
    • How do I start a timer after power-on, or when the input signal goes away?
    • How many instructions can be executed per sample in SigmaDSP?
    • Memory requirements for booting a SigmaDSP with a microcontroller
    • Monitoring average and instantaneous signal levels
    • Playing audio samples in SigmaDSP
    • SigmaDSP PCB Layout Best Practices
    • SigmaDSP Products and Evaluation Boards - ROHS and REACH Compliance
    • SigmaStudio 3.4 Released
    • Updating SigmaDSP Parameter with a Microcontroller
    • Using two SigmaDSP evaluation boards simultaneously with one USBi board
    • Welcome to the SIGMADSP Processors and SIGMASTUDIO Development tool community
    • What are the number formats for SigmaDSP?
    • What is the step size for audio delay in a SigmaDSP?
    • What types of capacitors are good to use in the analog audio signal path?
    • Where can I buy a SigmaDSP Evaluation Board or USBi (EVAL-ADUSB2EBZ)?
    • Which SigmaDSP ICs support selfbooting from an EEPROM?
    • Which SPI Mode is used by SigmaDSP Devices?
    • Why isn't a software/documentation CD included with my evaluation board?
  • +SigmaStudio: FAQ
  • +single precision VS double precision: FAQ
  • +Stimulus-Probe Capability and Limitations: FAQ
  • +Stopwatch to Count Successive Samples: FAQ
  • +Toolbox into the schematic tab: FAQ
  • +USB communications between the PC and SigmaDSP: FAQ
  • +Using Hierarchy Boards to create re-usable code: FAQ
  • New SigmaStudio 3.2.0 beta version available
  • SigmaStudio 3.3 Released
  • SigmaStudio 3.9.2 Beta Available for Download
  • SigmaStudio Rev 3.15.2 Bug Report for SPI EEPROM Write Speed

Can I use SigmaDSP to decode MP3/WAV/AAC?

Question:

I have read through SigmaDSP datasheet, and I find no related information on the MP3/WAV/AAC decoding engine for SigmaDSP.

Is there any available audio decoder for SigmaDSP like those modules for Blackfin?

Also, is there support for formats like Dolby AC3?

___________________________________________________

Answer:

The SigmaDSP's core is not capable of frequency domain processing, and therefore it cannot be used to decode/encode MP3/WAV/AAC like the Blackfin or Sharc. SigmaDSP simply takes linear PCM data in and processes it before outputting it as linear PCM data. It is therefore usually referred to as a "post-processor", since it is not involved in any tasks other than audio signal processing.

___________________________________________________

This FAQ was generated from the following discussion: Can I use SigmaDSP to decode MP3/WAV/AAC?

Tags: aac wav ac3 mp3 SigmaDSP
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: Can I use SigmaDSP to decode MP3/WAV/AAC?
    ADIApproved
    SigmaDSP's core is not capable of frequency domain processing, and therefore it cannot be used to decode/encode MP3/WAV/AAC like the Blackfin or Sharc. SigmaDSP simply takes linear PCM data in and processes...
  • Can I use SigmaDSP to decode MP3/WAV/AAC?
    cklooi
    I have read through sigmaDSP datasheet, and i find no related information on the Mp3/wav/aac decoding engine for SigmaDSP. Is there any available audio decoder for sigmaDSP like those modules for blackfin...
  • MP3 decoder for SigmaDSP
    takumi3952
    Hi, I understand MP3 decoder is not implemented in SigmaDSP standard library. Is there any 3rd party vendor for SigmaDSP MP3 decoder ? Thanks and Regards,
 
Related Content
  • RE: Can I use SigmaDSP to decode MP3/WAV/AAC?
    ADIApproved
    SigmaDSP's core is not capable of frequency domain processing, and therefore it cannot be used to decode/encode MP3/WAV/AAC like the Blackfin or Sharc. SigmaDSP simply takes linear PCM data in and processes...
  • Can I use SigmaDSP to decode MP3/WAV/AAC?
    cklooi
    I have read through sigmaDSP datasheet, and i find no related information on the Mp3/wav/aac decoding engine for SigmaDSP. Is there any available audio decoder for sigmaDSP like those modules for blackfin...
  • MP3 decoder for SigmaDSP
    takumi3952
    Hi, I understand MP3 decoder is not implemented in SigmaDSP standard library. Is there any 3rd party vendor for SigmaDSP MP3 decoder ? Thanks and Regards,